I am trying to follow the OpenSDA directions and my device will not show up as an MSD and will not go into bootloader mode. I am using windows 8, downloaded the PE drivers, and not sure what else I am missing for getting this to work. Any suggestions?
It was a cable issue. Used a different cable and it worked fine.
Hi Andrew,
can you see the "PEMicro OpenSDA Debug Driver" on the device manager window after you connected the USB cable to the FRDM board?
If you can see it, the "BOOTLOADER" MSD will appear when connected the cable with pushing the reset switch.
Didn't you go to this stage?
Anyway to use MSD, you should update the bootloader firmware on Windows 7 PC.
Best regards,
Yasuhiko Koumoto.
After connecting the device via USB, the PEMICRO OpenSDA Debug Driver does not appear. Is this something I am missing on windows? I have installed the PE Windows USB Drivers on windows 8.
Hi Andrew,
let me confirm. Did you got the PEDriver from P&E Microcomputer Systems of which title is as the following?
Windows USB Drivers
Download 「PEDrivers_install.exe」 for manual install.
Version 11.1, updated November 2, 2012.
I could have installed it successfully on both Windows8 and Windows7. You would not go further until the driver was installed.
I cannot guess the reason why you failed to install it.
Best regards,
Yasuhiko Koumoto.
I have installed that driver on my C drive. All of the text logs I have looked in say the driver install was successful as well. When I connect the device, the PEMicro OpenSDA Debug Driver does not show up. Is it a separate driver I need to install?
This is what I see before and after plugging in the FRDM-board. (Even after refreshing the screen).
Hi Andrew,
are there any differences from my environment? The below is my C drive.
$ ls -lR PEMicro/
PEMicro/:
合計 4
drwx------+ 1 Administrators なし 0 7月 26 2014 PEDriversPEMicro/PEDrivers:
合計 72
drwx------+ 1 Administrators なし 0 7月 26 2014 Drivers_11_1_1
-rwx------+ 1 Administrators なし 5482 8月 20 2010 license_prog.pdf
-rwx------+ 1 Administrators なし 62958 7月 26 2014 uninstall.exePEMicro/PEDrivers/Drivers_11_1_1:
合計 8
drwx------+ 1 Administrators なし 0 7月 26 2014 osbdm
drwx------+ 1 Administrators なし 0 7月 26 2014 windriverPEMicro/PEDrivers/Drivers_11_1_1/osbdm:
合計 20
-rwx------+ 1 Administrators なし 8391 2月 14 2013 osbdm_opensda_drivers.cat
-rwx------+ 1 Administrators なし 3095 2月 14 2013 pe_libusb_interface.inf
drwx------+ 1 Administrators なし 0 7月 26 2014 redist
-rwx------+ 1 Administrators なし 3346 2月 14 2013 serialcdc_interface.inf
drwx------+ 1 Administrators なし 0 7月 26 2014 utilPEMicro/PEDrivers/Drivers_11_1_1/osbdm/redist:
合計 92
-rwx------+ 1 Administrators なし 46528 7月 29 2010 libusb0.dll
-rwx------+ 1 Administrators なし 42944 7月 29 2010 libusb0.sysPEMicro/PEDrivers/Drivers_11_1_1/osbdm/util:
合計 664
-rwx------+ 1 Administrators なし 677952 7月 14 2009 dpinst_64.exePEMicro/PEDrivers/Drivers_11_1_1/windriver:
合計 972
-rwx------+ 1 Administrators なし 525792 11月 2 2006 difxapi.dll
-rwx------+ 1 Administrators なし 5014 2月 14 2013 pe_winusb_interface.inf
-rwx------+ 1 Administrators なし 4736 7月 26 2014 pe_winusb_interface.log
-rwx------+ 1 Administrators なし 8756 2月 14 2013 pemicro11.cat
drwx------+ 1 Administrators なし 0 7月 26 2014 redist
-rwx------+ 1 Administrators なし 8472 8月 26 2012 wd1110.cat
-rwx------+ 1 Administrators なし 146432 8月 26 2012 wdreg_gui.exe
-rwx------+ 1 Administrators なし 2316 8月 26 2012 windrvr6.inf
-rwx------+ 1 Administrators なし 266752 8月 26 2012 windrvr6.sys
-rwx------+ 1 Administrators なし 2822 7月 26 2014 windrvr6_install.logPEMicro/PEDrivers/Drivers_11_1_1/windriver/redist:
合計 1568
-rwx------+ 1 Administrators なし 408240 10月 17 2009 peusba05.dll
-rwx------+ 1 Administrators なし 442544 9月 11 2012 peusba06.dll
-rwx------+ 1 Administrators なし 148144 10月 17 2009 peusbb05.dll
-rwx------+ 1 Administrators なし 110592 8月 26 2012 peusbb06.dll
-rwx------+ 1 Administrators なし 434352 10月 17 2009 PEUSBMGR.dll
-rwx------+ 1 Administrators なし 45568 8月 26 2012 system64.exe
Best regards,
Yasuhiko Koumoto.
Everything is there. I have uninstalled and re-installed the driver 3 times as well. No luck. Do I need to open one of those files to get the driver to work? Or for the board to be recognized?
Hello Andrew:
I would like to help. Please answer some questions:
1) Do you see something under Ports (COM & LPT) in Device Manager?
2) The FRDM-KL43Z has 2 USB ports. Which one are you using?
3) Do you see the green LED (D8) ON when connecting the board?
4) Cannot you enter BOOTLOADER mode? This is done by holding reset button pressed and connecting the OpenSDA USB port.
5) Have you tried with a different computer, especially one with Windows 7?
6) Does you PC have an antivirus? If so, try disabling it momentarily.
These are just generic questions, I am trying to understand better your issue, so please be specific.
Regards!
Jorge Gonzalez
Hello Andrew,
let me confirm one more thing. I think it would be little possible thing but you didn't plug to wrong connector, did you?
I'm sorry to give a stupid confirmation.
Can you prepare Windows7 PC? You'd better try the same procedure on Windows7. To use OpenSDA (not v2) FRDM board on Windows8, the bootloader firmware update on Windows7 is mandatory. Anyway you must prepare the windows7 PC.
Or another scenario is your FRDM board would be a defeated part. Can you exchange it?
Best regards,
Yasuhiko Koumoto