FRDM K64 can’t run at 120Mhz

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM K64 can’t run at 120Mhz

1,887 次查看
mikesmith
Contributor I

Hi, I’m trying to use my K64 with a bareboard Project. So I decided to configure the system clock. I wanted to run the K64 at 120 MHz in PEE mode, but I failed, somebody can help me? I attached the code I’ve been using; My code works for frequencies below 66 MHz (at the output of MCGOUTCLK). I’m using the mcg diver that is provided by freescale.

Regard

 

Note: If I configure the PLL with correct values (PLL0_PRDIV=25 and PLL0_VDIV=50) for 120 Mhz the debugger gets lost

Original Attachment has been moved to: MCG_sources.rar

0 项奖励
回复
2 回复数

933 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

It is very probable that you need to set the correct values for the OUTDIV fields in the SIM_CLKDIV registers.

Regards,

Alejandro

0 项奖励
回复

933 次查看
BlackNight
NXP Employee
NXP Employee

The easiest way is if you have a look what settings Processor Expert is using. Have a look here:

FRDM-K64F at Maximum Speed of 120 MHz | MCU on Eclipse

I have pasted the code of CPU_Init.c so you can see what it does.

Erich

/** ###################################################################

**      Filename    : CPU_Init.c

**      Processor   : MK64FN1M0VLL12

**      Version     : 1.0

**      Abstract    :

**         This file implements the MCU initialization and CPU component runtime methods.

**

**     Copyright : 1997 - 2014 Freescale Semiconductor, Inc.

**     All Rights Reserved.

**   

**     Redistribution and use in source and binary forms, with or without modification,

**     are permitted provided that the following conditions are met:

**   

**     o Redistributions of source code must retain the above copyright notice, this list

**       of conditions and the following disclaimer.

**   

**     o Redistributions in binary form must reproduce the above copyright notice, this

**       list of conditions and the following disclaimer in the documentation and/or

**       other materials provided with the distribution.

**   

**     o Neither the name of Freescale Semiconductor, Inc. nor the names of its

**       contributors may be used to endorse or promote products derived from this

**       software without specific prior written permission.

**   

**     THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND

**     ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED

**     WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE

**     DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE FOR

**     ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES

**     (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES;

**     LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON

**     ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT

**     (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS

**     SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.

**   

**     http: www.freescale.com

**     mail: support@freescale.com

** ###################################################################*/

/*!

** @file CPU_Init.c                                                

** @version 01.00

** @brief

**         This file implements the MCU initialization and CPU component runtime methods.

*/       

/*!

**  @addtogroup CPU_Init_module CPU_Init module documentation

**  @{

*/       

/* MODULE CPU_Init.c */

#include "PE_Types.h"

#include "MK64F12.h"

#include "Init_Config.h"

#include "Peripherals_Init.h"

#include "CPU_Init.h"

#include "Vectors_Config.h"

#include "Events.h"

#ifdef __cplusplus

extern "C" {

#endif

#ifdef CPU_FLASH_CONFIG_FIELD

/* Flash configuration field */

  #if defined(__CWCC__)

/* Pragma to place the flash configuration field on correct location defined in linker file. */

#pragma define_section cfmconfig ".cfmconfig" ".cfmconfig" ".cfmconfig" far_abs R

static __declspec(cfmconfig) uint8_t _cfm[0x10] = {CPU_FLASH_CONFIG_FIELD};

  #elif defined(__IAR_SYSTEMS_ICC__)  

/* Pragma to place the flash configuration field on correct location defined in linker file. */

#pragma language=extended

#pragma location = "FlashConfig"

__root const uint8_t Config[0x10] @ "FlashConfig" = {CPU_FLASH_CONFIG_FIELD};

  #elif defined(__GNUC__)

__attribute__ ((section (".cfmconfig"))) const uint8_t _cfm[0x10] = {CPU_FLASH_CONFIG_FIELD};

  #elif defined(__CC_ARM)

__attribute__ ((section (".cfmconfig"))) const uint8_t _cfm[0x10] __attribute__((used)) = {CPU_FLASH_CONFIG_FIELD};

  #else

    #error Unsupported compiler!

  #endif

#endif  

extern void Common_Init(void);         /* Forward declaration of generated common initialization in generated CPU module */

extern void Components_Init(void);     /* Forward declaration of generated LDD components initialization in generated CPU module */

extern void LDD_SetClockConfiguration(LDD_TClockConfiguration ClockConfiguration);

/* Global variables */

volatile uint8_t SR_reg;               /* Current value of the FAULTMASK register */

volatile uint8_t SR_lock = 0x00U;      /* Lock */

LDD_TClockConfiguration ClockConfigurationID = CPU_CLOCK_CONFIG_0; /* Active clock configuration */

static const CPU_TClockGenMode ClockGenModeMatrix[8][8] = {

/* This matrix defines which mode is next in the MCG Mode state diagram in transitioning from the

   current mode to a target mode*/

  { CPU_MCG_MODE_FEI,  CPU_MCG_MODE_FBI,  CPU_MCG_MODE_FBI,  CPU_MCG_MODE_FEE,  CPU_MCG_MODE_FBE,  CPU_MCG_MODE_FBE,  CPU_MCG_MODE_FBE,  CPU_MCG_MODE_FBE  }, /* FEI */

  { CPU_MCG_MODE_FEI,  CPU_MCG_MODE_FBI,  CPU_MCG_MODE_BLPI, CPU_MCG_MODE_FEE,  CPU_MCG_MODE_FBE,  CPU_MCG_MODE_FBE,  CPU_MCG_MODE_FBE,  CPU_MCG_MODE_FBE  }, /* FBI */

  { CPU_MCG_MODE_FBI,  CPU_MCG_MODE_FBI,  CPU_MCG_MODE_BLPI, CPU_MCG_MODE_FBI,  CPU_MCG_MODE_FBI,  CPU_MCG_MODE_FBI,  CPU_MCG_MODE_FBI,  CPU_MCG_MODE_FBI  }, /* BLPI */

  { CPU_MCG_MODE_FEI,  CPU_MCG_MODE_FBI,  CPU_MCG_MODE_FBI,  CPU_MCG_MODE_FEE,  CPU_MCG_MODE_FBE,  CPU_MCG_MODE_FBE,  CPU_MCG_MODE_FBE,  CPU_MCG_MODE_FBE  }, /* FEE */

  { CPU_MCG_MODE_FEI,  CPU_MCG_MODE_FBI,  CPU_MCG_MODE_FBI,  CPU_MCG_MODE_FEE,  CPU_MCG_MODE_FBE,  CPU_MCG_MODE_BLPE, CPU_MCG_MODE_PBE,  CPU_MCG_MODE_PBE  }, /* FBE */

  { CPU_MCG_MODE_FBE,  CPU_MCG_MODE_FBE,  CPU_MCG_MODE_FBE,  CPU_MCG_MODE_FBE,  CPU_MCG_MODE_FBE,  CPU_MCG_MODE_BLPE, CPU_MCG_MODE_PBE,  CPU_MCG_MODE_PBE  }, /* BLPE */

  { CPU_MCG_MODE_FBE,  CPU_MCG_MODE_FBE,  CPU_MCG_MODE_FBE,  CPU_MCG_MODE_FBE,  CPU_MCG_MODE_FBE,  CPU_MCG_MODE_BLPE, CPU_MCG_MODE_PBE,  CPU_MCG_MODE_PEE  }, /* PBE */

  { CPU_MCG_MODE_PBE,  CPU_MCG_MODE_PBE,  CPU_MCG_MODE_PBE,  CPU_MCG_MODE_PBE,  CPU_MCG_MODE_PBE,  CPU_MCG_MODE_PBE,  CPU_MCG_MODE_PBE,  CPU_MCG_MODE_PEE  }  /* PEE */

};

static const CPU_TClockConfigDescriptor CPU_ClockConfigDescriptors[CPU_CLOCK_CONFIG_NUMBER] = {

  #if defined(CPU_CLOCK_CONFIG_0)

  /* Clock configuration 0 */

  {

    CPU_MCG_MODE_CONFIG_0,             /* Clock generator mode */

    CPU_CLOCK_PMODE_CONFIG_0,          /* Very low power mode enable/disable */

    {                                  /* MCG registers */

      CPU_MCG_C1_CONFIG_0,CPU_MCG_C2_CONFIG_0,CPU_MCG_C4_CONFIG_0,CPU_MCG_C5_CONFIG_0,CPU_MCG_C6_CONFIG_0,CPU_MCG_SC_CONFIG_0,CPU_OSC_CR_CONFIG_0,

    },

    {                                  /* SIM registers */

      CPU_SIM_SOPT1_CONFIG_0,CPU_SIM_SOPT2_CONFIG_0,CPU_SIM_CLKDIV1_CONFIG_0,

    },

    CPU_BUS_CLK_HZ_CONFIG_0            /* Bus frequency */

  }

  #endif

  #if defined(CPU_CLOCK_CONFIG_1)

  /* Clock configuration 1 */

  ,{

    CPU_MCG_MODE_CONFIG_1,             /* Clock generator mode */

    CPU_CLOCK_PMODE_CONFIG_1,          /* Very low power mode enable/disable */

    {                                  /* MCG registers */

      CPU_MCG_C1_CONFIG_1,CPU_MCG_C2_CONFIG_1,CPU_MCG_C4_CONFIG_1,CPU_MCG_C5_CONFIG_1,CPU_MCG_C6_CONFIG_1,CPU_MCG_SC_CONFIG_1,CPU_OSC_CR_CONFIG_1,

    },

    {                                  /* SIM registers */

      CPU_SIM_SOPT1_CONFIG_1,CPU_SIM_SOPT2_CONFIG_1,CPU_SIM_CLKDIV1_CONFIG_1,

    },

    CPU_BUS_CLK_HZ_CONFIG_1            /* Bus frequency */

  }

  #endif

  #if defined(CPU_CLOCK_CONFIG_2)

  /* Clock configuration 2 */

  ,{

    CPU_MCG_MODE_CONFIG_2,             /* Clock generator mode */

    CPU_CLOCK_PMODE_CONFIG_2,          /* Very low power mode enable/disable */

    {                                  /* MCG registers */

      CPU_MCG_C1_CONFIG_2,CPU_MCG_C2_CONFIG_2,CPU_MCG_C4_CONFIG_2,CPU_MCG_C5_CONFIG_2,CPU_MCG_C6_CONFIG_2,CPU_MCG_SC_CONFIG_2,CPU_OSC_CR_CONFIG_2,

    },

    {                                  /* SIM registers */

      CPU_SIM_SOPT1_CONFIG_2,CPU_SIM_SOPT2_CONFIG_2,CPU_SIM_CLKDIV1_CONFIG_2,

    },

    CPU_BUS_CLK_HZ_CONFIG_2            /* Bus frequency */

  }

  #endif

  #if defined(CPU_CLOCK_CONFIG_3)

  /* Clock configuration 3 */

  ,{

    CPU_MCG_MODE_CONFIG_3,             /* Clock generator mode */

    CPU_CLOCK_PMODE_CONFIG_3,          /* Very low power mode enable/disable */

    {                                  /* MCG registers */

      CPU_MCG_C1_CONFIG_3,CPU_MCG_C2_CONFIG_3,CPU_MCG_C4_CONFIG_3,CPU_MCG_C5_CONFIG_3,CPU_MCG_C6_CONFIG_3,CPU_MCG_SC_CONFIG_3,CPU_OSC_CR_CONFIG_3,

    },

    {                                  /* SIM registers */

      CPU_SIM_SOPT1_CONFIG_3,CPU_SIM_SOPT2_CONFIG_3,CPU_SIM_CLKDIV1_CONFIG_3,

    },

    CPU_BUS_CLK_HZ_CONFIG_3            /* Bus frequency */

  }

  #endif

  #if defined(CPU_CLOCK_CONFIG_4)

  /* Clock configuration 4 */

  ,{

    CPU_MCG_MODE_CONFIG_4,             /* Clock generator mode */

    CPU_CLOCK_PMODE_CONFIG_4,          /* Very low power mode enable/disable */

    {                                  /* MCG registers */

      CPU_MCG_C1_CONFIG_4,CPU_MCG_C2_CONFIG_4,CPU_MCG_C4_CONFIG_4,CPU_MCG_C5_CONFIG_4,CPU_MCG_C6_CONFIG_4,CPU_MCG_SC_CONFIG_4,CPU_OSC_CR_CONFIG_4,

    },

    {                                  /* SIM registers */

      CPU_SIM_SOPT1_CONFIG_4,CPU_SIM_SOPT2_CONFIG_4,CPU_SIM_CLKDIV1_CONFIG_4,

    },

    CPU_BUS_CLK_HZ_CONFIG_4            /* Bus frequency */

  }

  #endif

  #if defined(CPU_CLOCK_CONFIG_5)

  /* Clock configuration 5 */

  ,{

    CPU_MCG_MODE_CONFIG_5,             /* Clock generator mode */

    CPU_CLOCK_PMODE_CONFIG_5,          /* Very low power mode enable/disable */

    {                                  /* MCG registers */

      CPU_MCG_C1_CONFIG_5,CPU_MCG_C2_CONFIG_5,CPU_MCG_C4_CONFIG_5,CPU_MCG_C5_CONFIG_5,CPU_MCG_C6_CONFIG_5,CPU_MCG_SC_CONFIG_5,CPU_OSC_CR_CONFIG_5,

    },

    {                                  /* SIM registers */

      CPU_SIM_SOPT1_CONFIG_5,CPU_SIM_SOPT2_CONFIG_5,CPU_SIM_CLKDIV1_CONFIG_5,

    },

    CPU_BUS_CLK_HZ_CONFIG_5            /* Bus frequency */

  }

  #endif

  #if defined(CPU_CLOCK_CONFIG_6)

  /* Clock configuration 6 */

  ,{

    CPU_MCG_MODE_CONFIG_6,             /* Clock generator mode */

    CPU_CLOCK_PMODE_CONFIG_6,          /* Very low power mode enable/disable */

    {                                  /* MCG registers */

      CPU_MCG_C1_CONFIG_6,CPU_MCG_C2_CONFIG_6,CPU_MCG_C4_CONFIG_6,CPU_MCG_C5_CONFIG_6,CPU_MCG_C6_CONFIG_6,CPU_MCG_SC_CONFIG_6,CPU_OSC_CR_CONFIG_6,

    },

    {                                  /* SIM registers */

      CPU_SIM_SOPT1_CONFIG_6,CPU_SIM_SOPT2_CONFIG_6,CPU_SIM_CLKDIV1_CONFIG_6,

    },

    CPU_BUS_CLK_HZ_CONFIG_6            /* Bus frequency */

  }

  #endif

  #if defined(CPU_CLOCK_CONFIG_7)

  /* Clock configuration 7 */

  ,{

    CPU_MCG_MODE_CONFIG_7,             /* Clock generator mode */

    CPU_CLOCK_PMODE_CONFIG_7,          /* Very low power mode enable/disable */

    {                                  /* MCG registers */

      CPU_MCG_C1_CONFIG_7,CPU_MCG_C2_CONFIG_7,CPU_MCG_C4_CONFIG_7,CPU_MCG_C5_CONFIG_7,CPU_MCG_C6_CONFIG_7,CPU_MCG_SC_CONFIG_7,CPU_OSC_CR_CONFIG_7,

    },

    {                                  /* SIM registers */

      CPU_SIM_SOPT1_CONFIG_7,CPU_SIM_SOPT2_CONFIG_7,CPU_SIM_CLKDIV1_CONFIG_7,

    },

    CPU_BUS_CLK_HZ_CONFIG_7            /* Bus frequency */

  }

  #endif

};

static const CPU_TClockGenRegs CPU_DefaultFEI = {

  CPU_DEFAULT_FEI_MCG_C1,CPU_DEFAULT_FEI_MCG_C2,CPU_DEFAULT_FEI_MCG_C4,CPU_DEFAULT_FEI_MCG_C5,CPU_DEFAULT_FEI_MCG_C6,CPU_DEFAULT_FEI_MCG_SC,CPU_DEFAULT_FEI_OSC_CR

};

static const CPU_TClockGenRegs CPU_DefaultFBI = {

  CPU_DEFAULT_FBI_MCG_C1,CPU_DEFAULT_FBI_MCG_C2,CPU_DEFAULT_FBI_MCG_C4,CPU_DEFAULT_FBI_MCG_C5,CPU_DEFAULT_FBI_MCG_C6,CPU_DEFAULT_FBI_MCG_SC,CPU_DEFAULT_FBI_OSC_CR

};

static const CPU_TClockGenRegs CPU_DefaultBLPI = {

  CPU_DEFAULT_BLPI_MCG_C1,CPU_DEFAULT_BLPI_MCG_C2,CPU_DEFAULT_BLPI_MCG_C4,CPU_DEFAULT_BLPI_MCG_C5,CPU_DEFAULT_BLPI_MCG_C6,CPU_DEFAULT_BLPI_MCG_SC,CPU_DEFAULT_BLPI_OSC_CR

};

static const CPU_TClockGenRegs CPU_DefaultFEE = {

  CPU_DEFAULT_FEE_MCG_C1,CPU_DEFAULT_FEE_MCG_C2,CPU_DEFAULT_FEE_MCG_C4,CPU_DEFAULT_FEE_MCG_C5,CPU_DEFAULT_FEE_MCG_C6,CPU_DEFAULT_FEE_MCG_SC,CPU_DEFAULT_FEE_OSC_CR

};

static const CPU_TClockGenRegs CPU_DefaultFBE = {

  CPU_DEFAULT_FBE_MCG_C1,CPU_DEFAULT_FBE_MCG_C2,CPU_DEFAULT_FBE_MCG_C4,CPU_DEFAULT_FBE_MCG_C5,CPU_DEFAULT_FBE_MCG_C6,CPU_DEFAULT_FBE_MCG_SC,CPU_DEFAULT_FBE_OSC_CR

};

static const CPU_TClockGenRegs CPU_DefaultBLPE = {

  CPU_DEFAULT_BLPE_MCG_C1,CPU_DEFAULT_BLPE_MCG_C2,CPU_DEFAULT_BLPE_MCG_C4,CPU_DEFAULT_BLPE_MCG_C5,CPU_DEFAULT_BLPE_MCG_C6,CPU_DEFAULT_BLPE_MCG_SC,CPU_DEFAULT_BLPE_OSC_CR

};

static const CPU_TClockGenRegs CPU_DefaultPBE = {

  CPU_DEFAULT_PBE_MCG_C1,CPU_DEFAULT_PBE_MCG_C2,CPU_DEFAULT_PBE_MCG_C4,CPU_DEFAULT_PBE_MCG_C5,CPU_DEFAULT_PBE_MCG_C6,CPU_DEFAULT_PBE_MCG_SC,CPU_DEFAULT_PBE_OSC_CR

};

static const CPU_TClockGenRegs CPU_DefaultPEE = {

  CPU_DEFAULT_PEE_MCG_C1,CPU_DEFAULT_PEE_MCG_C2,CPU_DEFAULT_PEE_MCG_C4,CPU_DEFAULT_PEE_MCG_C5,CPU_DEFAULT_PEE_MCG_C6,CPU_DEFAULT_PEE_MCG_SC,CPU_DEFAULT_PEE_OSC_CR

};

static const CPU_TClockGenRegs *const CPU_ClockGenModeRegs[CPU_MCG_MODES] = {

  &CPU_DefaultFEI,

  &CPU_DefaultFBI,

  &CPU_DefaultBLPI,

  &CPU_DefaultFEE,

  &CPU_DefaultFBE,

  &CPU_DefaultBLPE,

  &CPU_DefaultPBE,

  &CPU_DefaultPEE

};

/*

** ===================================================================

**     Method      :  Cpu_SetBASEPRI (component MK64FN1M0LL12)

**

**     Description :

**         This method sets the BASEPRI core register.

**         This method is internal. It is used by Processor Expert only.

** ===================================================================

*/

/*lint -save  -e586 -e950 Disable MISRA rule (2.1,1.1) checking. */

#if defined(_lint)

  #define CPU_SetBASEPRI(Level)  /* empty */

#elif defined(__CWCC__)

asm void CPU_SetBASEPRI(register uint32_t Level) {

  MSR BASEPRI,R0;

  MOV PC,LR

}

#elif defined(__GNUC__)

void CPU_SetBASEPRI(uint32_t Level) {

  __asm ("msr basepri, %[input]"::[input] "r" (Level):);

}

#elif defined(__CC_ARM)

__asm CPU_SetBASEPRI(uint32_t Level) {

  MSR BASEPRI,R0

  BX  LR

}

#endif

/*lint -restore Enable MISRA rule (2.1,1.1) checking. */

/*

** ===================================================================

**     Method      :  __init_hardware (component MK64FN1M0LL12)

**

**     Description :

**         This method is called from the _startup() function and

**         provides necessary system initialization such as PLL, and

**         external bus.

**         This method is internal. It is used by Processor Expert only.

** ===================================================================

*/

#if !defined(PEX_ENTRYPOINT_FUNCTION)

  #if defined(__IAR_SYSTEMS_ICC__)

    #define PEX_ENTRYPOINT_FUNCTION __low_level_init

  #elif defined(__CWCC__) | defined(__GNUC__) | defined(__CC_ARM)

    #define PEX_ENTRYPOINT_FUNCTION __init_hardware

  #endif

#endif /* !defined(PEX_ENTRYPOINT_FUNCTION) */

#if !defined(PEX_ENTRYPOINT_FUNCTION_TYPE)

  #if defined(__IAR_SYSTEMS_ICC__)

    #define PEX_ENTRYPOINT_FUNCTION_TYPE int

  #elif defined(__CWCC__) | defined(__GNUC__) | defined(__CC_ARM)

    #define PEX_ENTRYPOINT_FUNCTION_TYPE void

  #endif

#endif /* !defined(PEX_ENTRYPOINT_FUNCTION_TYPE) */

#if !defined(PEX_ENTRYPOINT_FUNCTION_RETURN)

  #if defined(__IAR_SYSTEMS_ICC__)  

    #define PEX_ENTRYPOINT_FUNCTION_RETURN return 1;

  #endif

#endif

PEX_ENTRYPOINT_FUNCTION_TYPE PEX_ENTRYPOINT_FUNCTION()

{

  /* Interrupt vector placement initialization */

  #if PEX_VECTOR_TABLE

    #if defined(__IAR_SYSTEMS_ICC__)

  SCB_VTOR = (uint32_t)(&__vector_table); /* Set the interrupt vector table position */

    #elif defined(__CWCC__) | defined(__GNUC__) | defined(__CC_ARM)

  SCB_VTOR = (uint32_t)(&__vect_table); /* Set the interrupt vector table position */

    #endif

  #endif

  /* Disable the WDOG module */

  #if STARTUP_WDOG

  WDOG_UNLOCK = (uint16_t)STARTUP_WDOG_KEY_1; /* Key 1 */

  WDOG_UNLOCK = (uint16_t)STARTUP_WDOG_KEY_2; /* Key 2 */

  WDOG_STCTRLH = (uint16_t)STARTUP_WDOG_STCTRLH_VALUE; /* Disable WDOG */

  #endif /* STARTUP_WDOG */

  /* System clock initialization */

#if STARTUP_RTCOSC

  /* SIM_SCGC6: RTC=1 */

  SIM_SCGC6 |= SIM_SCGC6_RTC_MASK;

  if ((RTC_CR & RTC_CR_OSCE_MASK) == 0u) { /* Only if the OSCILLATOR is not already enabled */

    RTC_CR = (uint32_t)((RTC_CR & (uint32_t)~(uint32_t)(RTC_CR_SC2P_MASK | RTC_CR_SC4P_MASK | RTC_CR_SC8P_MASK | RTC_CR_SC16P_MASK)) | (uint32_t)STARTUP_RTC_CR_SC_VALUE);

    RTC_CR |= (uint32_t)RTC_CR_OSCE_MASK;

    RTC_CR &= (uint32_t)~(uint32_t)RTC_CR_CLKO_MASK;

  }

#endif

  

  /* Internal reference clock trim initialization */

  #if (defined(STARTUP_CLOCK_INTERNAL_SLOW_TRIM_ADDRESS) || defined(STARTUP_CLOCK_INTERNAL_SLOW_FINE_TRIM_ADDRESS))

    #if defined(STARTUP_CLOCK_INTERNAL_SLOW_TRIM_ADDRESS)

  if ( *((uint8_t*)STARTUP_CLOCK_INTERNAL_SLOW_TRIM_ADDRESS) != 0xFFU) { /* Skip if non-volatile flash memory is erased */

    MCG_C3 = *((uint8_t*)STARTUP_CLOCK_INTERNAL_SLOW_TRIM_ADDRESS);

    #endif /* defined(STARTUP_CLOCK_INTERNAL_SLOW_TRIM_ADDRESS) */

    #if defined(STARTUP_CLOCK_INTERNAL_SLOW_FINE_TRIM_ADDRESS)

      #if defined(STARTUP_CLOCK_INTERNAL_FAST_TRIM_ADDRESS)

        #if (STARTUP_CLOCK_INTERNAL_FAST_TRIM_ADDRESS == STARTUP_CLOCK_INTERNAL_SLOW_FINE_TRIM_ADDRESS)

    MCG_C4 = (MCG_C4 & ~(MCG_C4_FCTRIM_MASK | MCG_C4_SCFTRIM_MASK)) |

             ((*((uint8_t*) STARTUP_CLOCK_INTERNAL_FAST_TRIM_ADDRESS)) & (MCG_C4_FCTRIM_MASK | MCG_C4_SCFTRIM_MASK));

        #else /* (STARTUP_CLOCK_INTERNAL_FAST_TRIM_ADDRESS == STARTUP_CLOCK_INTERNAL_SLOW_FINE_TRIM_ADDRESS) */

    MCG_C4 = (MCG_C4 & ~(MCG_C4_FCTRIM_MASK | MCG_C4_SCFTRIM_MASK)) |

             ((*((uint8_t*) STARTUP_CLOCK_INTERNAL_FAST_TRIM_ADDRESS)) & MCG_C4_FCTRIM_MASK) |

             ((*((uint8_t*) STARTUP_CLOCK_INTERNAL_SLOW_FINE_TRIM_ADDRESS)) & MCG_C4_SCFTRIM_MASK);

        #endif /* (STARTUP_CLOCK_INTERNAL_FAST_TRIM_ADDRESS == STARTUP_CLOCK_INTERNAL_SLOW_FINE_TRIM_ADDRESS) */

        #if defined(STARTUP_CLOCK_INTERNAL_FAST_FINE_TRIM_ADDRESS)

    MCG_C2 = (MCG_C2 & ~(MCG_C2_FCFTRIM_MASK)) | ((*((uint8_t*)STARTUP_CLOCK_INTERNAL_FAST_TRIM_ADDRESS)) & MCG_C2_FCFTRIM_MASK);

        #endif /* defined(STARTUP_CLOCK_INTERNAL_FAST_FINE_TRIM_ADDRESS) */

      #else /* defined(STARTUP_CLOCK_INTERNAL_FAST_TRIM_ADDRESS) */

    MCG_C4 = (MCG_C4 & ~(MCG_C4_SCFTRIM_MASK)) | ((*((uint8_t*)STARTUP_CLOCK_INTERNAL_SLOW_FINE_TRIM_ADDRESS)) & MCG_C4_SCFTRIM_MASK);

      #endif /* defined(STARTUP_CLOCK_INTERNAL_FAST_TRIM_ADDRESS) */

    #endif /* STARTUP_CLOCK_INTERNAL_SLOW_FINE_TRIM_ADDRESS */

    #if defined(STARTUP_CLOCK_INTERNAL_SLOW_TRIM_ADDRESS)

  }

    #endif /* defined(STARTUP_CLOCK_INTERNAL_SLOW_TRIM_ADDRESS) */

  #elif (defined(STARTUP_CLOCK_INTERNAL_FAST_TRIM_ADDRESS) || defined(STARTUP_CLOCK_INTERNAL_FAST_FINE_TRIM_ADDRESS))

    #if defined(STARTUP_CLOCK_INTERNAL_FAST_TRIM_ADDRESS)

  if ( *((uint8_t*)STARTUP_CLOCK_INTERNAL_FAST_TRIM_ADDRESS) != 0xFFU) { /* Skip if non-volatile flash memory is erased */

    MCG_C4 = (MCG_C4 & ~(MCG_C4_FCTRIM_MASK)) | ((*((uint8_t*)STARTUP_CLOCK_INTERNAL_FAST_TRIM_ADDRESS)) & MCG_C4_FCTRIM_MASK);

    #endif /* defined(STARTUP_CLOCK_INTERNAL_FAST_TRIM_ADDRESS) */

    #if defined(STARTUP_CLOCK_INTERNAL_FAST_FINE_TRIM_ADDRESS)

    MCG_C2 = (MCG_C2 & ~(MCG_C2_FCFTRIM_MASK)) | ((*((uint8_t*)STARTUP_CLOCK_INTERNAL_FAST_FINE_TRIM_ADDRESS)) & MCG_C2_FCFTRIM_MASK);

    #endif /* defined(STARTUP_CLOCK_INTERNAL_FAST_FINE_TRIM_ADDRESS) */

    #if defined(STARTUP_CLOCK_INTERNAL_FAST_TRIM_ADDRESS)

  }

    #endif /* defined(STARTUP_CLOCK_INTERNAL_FAST_TRIM_ADDRESS) */

  #endif /* STARTUP_CLOCK_INTERNAL_FAST_TRIM */

  /* SIM_CLKDIV1: OUTDIV1=0,OUTDIV2=1,OUTDIV3=4,OUTDIV4=4,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */

  SIM_CLKDIV1 = SIM_CLKDIV1_OUTDIV1(0x00) |

                SIM_CLKDIV1_OUTDIV2(0x01) |

                SIM_CLKDIV1_OUTDIV3(0x04) |

                SIM_CLKDIV1_OUTDIV4(0x04); /* Set the system prescalers to safe value */

  CPU_SetClockConfigGenMode(CPU_CLOCK_CONFIG_0);

  SIM_CLKDIV1 = (uint32_t)CPU_ClockConfigDescriptors[CPU_CLOCK_CONFIG_0].SysRegs.SIM_CLKDIV1_value; /* Update system prescalers */

  SIM_SOPT1 = (uint32_t)((SIM_SOPT1 & (uint32_t)~(uint32_t)SIM_SOPT1_OSC32KSEL_MASK) | (uint32_t)CPU_ClockConfigDescriptors[CPU_CLOCK_CONFIG_0].SysRegs.SIM_SOPT1_value); /* Update 32 kHz oscillator clock source (ERCLK32K) */

  SIM_SOPT2 = (uint32_t)((SIM_SOPT2 & (uint32_t)~(uint32_t)SIM_SOPT2_PLLFLLSEL_MASK) | (uint32_t)CPU_ClockConfigDescriptors[CPU_CLOCK_CONFIG_0].SysRegs.SIM_SOPT2_value); /* Update PLL/FLL clock select */

  #if defined(PEX_ENTRYPOINT_FUNCTION_RETURN)

  PEX_ENTRYPOINT_FUNCTION_RETURN

  #endif

}

/*

** ===================================================================

**     Method      :  PE_low_level_init (component MK64FN1M0LL12)

**

**     Description :

**         This method is internal. It is used by Processor Expert only.

** ===================================================================

*/

void PE_low_level_init(void)

{

  /* RTOS initialization */

  #ifdef PEX_RTOS_INIT

    PEX_RTOS_INIT();                   /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */

  #endif

  /* NMI, reset and debug pins port clock gate enable */

  #if CPU_NMI_PIN | CPU_RESET_PIN | CPU_SWD_DIO_PIN | CPU_SWD_CLK_PIN

  SIM_SCGC5 |= (uint32_t)SIM_SCGC5_PORTA_MASK; /* NMI and reset pin clock gate enable */

  #endif /* CPU_NMI_PIN | CPU_RESET_PIN */

  /* Non-maskable interrupt pin initialization */

  #if CPU_NMI_PIN

  /* Non-maskable interrupt pin routing */

  /* PORTA_PCR4: ISF=0,MUX=7 */

  PORTA_PCR4 = (uint32_t)((PORTA_PCR4 & (uint32_t)~(uint32_t)(

                PORT_PCR_ISF_MASK

               )) | (uint32_t)(

                PORT_PCR_MUX(0x07)

               ));

  #endif /* CPU_NMI_PIN */

  /* JTAG TDI pin initialization */

  #if CPU_JTAG_TDI_PIN

  /* JTAG TDI pin routing */

  #endif /* CPU_JTAG_TDI_PIN */

  /* JTAG TDO pin initialization */

  #if CPU_JTAG_TDO_PIN

  /* JTAG TDO pin routing */

  #endif /* CPU_JTAG_TDO_PIN */

  /* JTAG TDO pin initialization */

  #if CPU_JTAG_TCK_PIN

  /* JTAG TCK pin routing */

  #endif /* CPU_JTAG_TCK_PIN */

  

    /* JTAG TMS pin initialization */

  #if CPU_JTAG_TMS_PIN

  /* JTAG TMS pin routing */

  #endif /* CPU_JTAG_TMS_PIN */

    /* JTAG TRST pin initialization */

  #if CPU_JTAG_TRST_PIN

  /* JTAG nTRST pin routing */

  #endif /* CPU_JTAG_TRST_PIN */

  /* Low power modes protection */

  /* Disable very low power mode protection */

  SMC_PMPROT = (CPU_LOW_POWER_ALLOW_VLP? SMC_PMPROT_AVLP_MASK : 0) |

               (CPU_LOW_POWER_ALLOW_LLS? SMC_PMPROT_ALLS_MASK : 0) |

               (CPU_LOW_POWER_ALLOW_VLLS? SMC_PMPROT_AVLLS_MASK : 0);

  /* Common initialization */

  #if CPU_COMMON_INIT

  Common_Init();

  #endif /* CPU_COMMON_INIT */

  /* Peripheral initialization components initialization */

  #if CPU_PERIPHERALS_INIT

  Peripherals_Init();

  #endif /* CPU_PERIPHERALS_INIT */

  /* OnReset event */

  #ifdef CPU_ON_RESET_EVENT_NAME

  CPU_ON_RESET_EVENT_NAME((uint16_t)(((uint16_t)RCM_SRS1) << 8U) | (uint16_t)RCM_SRS0); /* Invoke an user event */

  #endif /* CPU_ON_RESET_EVENT_NAME */

  /* Rest of components initialization */

  #if CPU_COMPONENTS_INIT

  Components_Init();

  #endif /* CPU_COMPONENTS_INIT */

  /* Interrupts priority level initialization */

   #if (CPU_INT_PRIORITY == 0)

   __DI();

  #else /* (CPU_INT_PRIORITY == 0) */

    #if defined(__IAR_SYSTEMS_ICC__)

    __set_BASEPRI(CPU_INT_PRIORITY);

    #elif defined(__CWCC__)

    CPU_SetBASEPRI(CPU_INT_PRIORITY);

    #elif defined(__GNUC__)

    CPU_SetBASEPRI(CPU_INT_PRIORITY);

    #elif defined(__CC_ARM)

    CPU_SetBASEPRI(CPU_INT_PRIORITY);

      #else /* defined(compiler ID) */

        #error Unsupported compiler

      #endif /* defined(compiler ID) */

  #endif

}

CPU_TClockGenMode CPU_GetClockGenMode(void)

{

  switch (MCG_C1  & MCG_C1_CLKS_MASK) {

    case  0x00U:

      /* Output of FLL or PLL is selected */

      if ((MCG_C6 & MCG_C6_PLLS_MASK) == 0x00U) {

        /* Output of FLL is selected */

        if ((MCG_C1 & MCG_C1_IREFS_MASK) == 0x00U) {

          /* External reference clock is selected */

          return CPU_MCG_MODE_FEE;

        } else {

          /* Internal reference clock is selected */

          return CPU_MCG_MODE_FEI;

        }

      } else {

        /* Output of FLL is selected */

          return CPU_MCG_MODE_PEE;

        }

    case 0x40U:

      /* Internal reference clock is selected */

      if ((MCG_C2 & MCG_C2_LP_MASK) == 0x00U) {

        /* Low power mode is disabled */

        return CPU_MCG_MODE_FBI;

      } else {

        /* Low power mode is enabled */

        return CPU_MCG_MODE_BLPI;

      }

    case 0x80U:

      /* External reference clock is selected */

      if ((MCG_C6 & MCG_C6_PLLS_MASK) == 0x00U) {

        /* FLL or PLL is selected */

        if ((MCG_C2 & MCG_C2_LP_MASK) == 0x00U) {

          /* FLL is selected */

          return CPU_MCG_MODE_FBE;

        } else {

          /* Low power mode is enabled */

          return CPU_MCG_MODE_BLPE;

        }

      } else {

        /* PLL is selected */

        return CPU_MCG_MODE_PBE;

      }

    default:

      return (CPU_TClockGenMode)0x00U;

  }

}

void CPU_SetClockConfigGenMode(LDD_TClockConfiguration ConfigID)

{

  CPU_TClockGenMode NextMode;

  CPU_TClockGenRegs NextModeRegs;

  CPU_TClockGenMode TargetMode = CPU_ClockConfigDescriptors[ConfigID].Mode;

  /* External clock source pin routing */

  if ((TargetMode & (CPU_CLOCK_EXTERNAL_CLOCK_MASK | CPU_CLOCK_EXTERNAL_CRYSTAL_MASK)) != 0) { /* Is external clock source used in targeted clock configuration? */

    /* If yes, initialize the EXTAL pin routing */

    SIM_SCGC5 |= (uint32_t)SIM_SCGC5_PORTA_MASK; /* Enable EXTAL/XTAL pins clock gate */

    /* PORTA_PCR18: ISF=0,MUX=0 */

    PORTA_PCR18 &= (uint32_t)~(uint32_t)(

                    PORT_PCR_ISF_MASK |

                    PORT_PCR_MUX(0x07)

                   );

    if ((TargetMode & CPU_CLOCK_EXTERNAL_CRYSTAL_MASK) != 0) { /* Is external crystal/resonator used in targeted clock configuration? */

      /* If yes, initialize also XTAL pin routing */

      /* PORTA_PCR19: ISF=0,MUX=0 */

      PORTA_PCR19 &= (uint32_t)~(uint32_t)(

                      PORT_PCR_ISF_MASK |

                      PORT_PCR_MUX(0x07)

                     );

    }

  }

  if ((MCG_SC & MCG_SC_FCRDIV_MASK) != CPU_ClockConfigDescriptors[ConfigID].GenRegs.MCG_SC_value) { /* Check if it is necessary to update Fast Clock Internal Reference Divider */

    if ((MCG_C2 & MCG_C2_IRCS_MASK) == 0x00U) {

      MCG_SC = (MCG_SC & (uint8_t)(~(MCG_SC_FCRDIV_MASK))) | CPU_ClockConfigDescriptors[ConfigID].GenRegs.MCG_SC_value;

    } else {

      if ((MCG_C1 & (MCG_C1_IREFS_MASK || MCG_C1_IRCLKEN_MASK)) != 0x00U) { /* Is internal reference clock active? */    

        MCG_C2 &= (uint8_t)(~(MCG_C2_IRCS_MASK)); /* Disable the fast internal clock */

        while((MCG_S & MCG_S_IRCST_MASK) != 0x00U) { /* Check that the source internal reference clock is slow clock. */

        }

        MCG_SC = (MCG_SC & (uint8_t)(~(MCG_SC_FCRDIV_MASK))) | CPU_ClockConfigDescriptors[ConfigID].GenRegs.MCG_SC_value;  

        MCG_C2 |= MCG_C2_IRCS_MASK;    /* Re-enable the fast internal clock */

        while((MCG_S & MCG_S_IRCST_MASK) == 0x00U) { /* Check that the source internal reference clock is fast clock. */

        }

      } else {

        MCG_C2 &= (uint8_t)(~(MCG_C2_IRCS_MASK)); /* Disable the fast internal clock */

        MCG_SC = (MCG_SC & (uint8_t)(~(MCG_SC_FCRDIV_MASK))) | CPU_ClockConfigDescriptors[ConfigID].GenRegs.MCG_SC_value;  

        MCG_C2 |= MCG_C2_IRCS_MASK;    /* Re-enable the fast internal clock */

      }

    }

  }    

  NextMode = CPU_GetClockGenMode(); /* Identify the currently active MCG mode */

  do {

    NextMode = ClockGenModeMatrix[NextMode & CPU_MCG_MODE_INDEX_MASK][TargetMode & CPU_MCG_MODE_INDEX_MASK];

    if (NextMode == (TargetMode & CPU_MCG_MODE_INDEX_MASK)) {

      NextModeRegs = CPU_ClockConfigDescriptors[ConfigID].GenRegs;

    } else {

      NextModeRegs = *CPU_ClockGenModeRegs[NextMode & CPU_MCG_MODE_INDEX_MASK];

    }

    switch (NextMode & CPU_MCG_MODE_INDEX_MASK) {

      case CPU_MCG_MODE_FEI:

      case CPU_MCG_MODE_FBI:

        MCG_C1 = NextModeRegs.MCG_C1_value; /* Set C1 (clock source selection, FLL ext. reference divider, int. reference enable etc.) */

        while((MCG_S & MCG_S_IREFST_MASK) == 0x00U) { /* Check that the source of the FLL reference clock is the internal reference clock. */

        }

        MCG_C2 = ((NextModeRegs.MCG_C2_value) & (uint8_t)(~(MCG_C2_FCFTRIM_MASK))) | (MCG_C2 & MCG_C2_FCFTRIM_MASK); /* Set C2 (freq. range, ext. and int. reference selection etc.; trim values not changed) */

        MCG_C4 = ((NextModeRegs.MCG_C4_value) & (uint8_t)(~(MCG_C4_FCTRIM_MASK | MCG_C4_SCFTRIM_MASK))) | (MCG_C4 & (MCG_C4_FCTRIM_MASK | MCG_C4_SCFTRIM_MASK)); /* Set C4 (FLL output; trim values not changed) */

        OSC_CR = NextModeRegs.OSC_CR_value; /* Set OSC_CR (OSCERCLK enable, oscillator capacitor load) */        

        if (TargetMode & CPU_CLOCK_RTC_OSC_MASK) {

          MCG_C7 = MCG_C7_OSCSEL(1);   /* Select RTC oscillator as MCG clock source */

        } else if (TargetMode & CPU_CLOCK_IRC48M_MASK) {

          MCG_C7 = MCG_C7_OSCSEL(2);   /* Select IRC 48MHz as MCG clock source */

        } else {

          MCG_C7 = 0;                  /* Select system oscillator as MCG clock source */

        }

        MCG_C5 = NextModeRegs.MCG_C5_value; /* Set C5 (PLL settings, PLL reference divider etc.) */

        if (TargetMode & CPU_CLOCK_PLL_MASK) {

          MCG_C5 |= MCG_C5_PLLCLKEN0_MASK;

        }

        MCG_C6 = NextModeRegs.MCG_C6_value; /* Set C6 (PLL select, VCO divider etc.) */

        break;

      case CPU_MCG_MODE_BLPI:

        MCG_C1 = NextModeRegs.MCG_C1_value; /* Set C1 (clock source selection, FLL ext. reference divider, int. reference enable etc.) */

        while((MCG_S & MCG_S_IREFST_MASK) == 0x00U) { /* Check that the source of the FLL reference clock is the internal reference clock. */

        }

        MCG_C2 = ((NextModeRegs.MCG_C2_value) & (uint8_t)(~(MCG_C2_FCFTRIM_MASK))) | (MCG_C2 & MCG_C2_FCFTRIM_MASK); /* Set C2 (freq. range, ext. and int. reference selection etc.; trim values not changed) */

        OSC_CR = NextModeRegs.OSC_CR_value; /* Set OSC_CR (OSCERCLK enable, oscillator capacitor load) */

        if (TargetMode & CPU_CLOCK_FAST_MASK) {

          while((MCG_S & MCG_S_IRCST_MASK) == 0x00U) { /* Check that the fast external reference clock is selected. */

            }

          }        

        break;

      case CPU_MCG_MODE_FEE:

      case CPU_MCG_MODE_FBE:

        MCG_C2 = ((NextModeRegs.MCG_C2_value) & (uint8_t)(~(MCG_C2_FCFTRIM_MASK))) | (MCG_C2 & MCG_C2_FCFTRIM_MASK); /* Set C2 (freq. range, ext. and int. reference selection etc.; trim values not changed) */

        OSC_CR = NextModeRegs.OSC_CR_value; /* Set OSC_CR (OSCERCLK enable, oscillator capacitor load) */        

        if (TargetMode & CPU_CLOCK_RTC_OSC_MASK) {

          MCG_C7 = MCG_C7_OSCSEL(1);   /* Select RTC oscillator as MCG clock source */

        } else if (TargetMode & CPU_CLOCK_IRC48M_MASK) {

          MCG_C7 = MCG_C7_OSCSEL(2);   /* Select IRC 48MHz as MCG clock source */

        } else {

          MCG_C7 = 0;                  /* Select system oscillator as MCG clock source */

        }

        MCG_C1 = NextModeRegs.MCG_C1_value; /* Set C1 (clock source selection, FLL ext. reference divider, int. reference enable etc.) */

        if ((TargetMode & CPU_CLOCK_EXTERNAL_CRYSTAL_MASK) != 0) {

          while((MCG_S & MCG_S_OSCINIT0_MASK) == 0x00U) { /* Check that the oscillator is running */

          }

        }

        while((MCG_S & MCG_S_IREFST_MASK) != 0x00U) { /* Check that the source of the FLL reference clock is the external reference clock. */

        }

        MCG_C4 = ((NextModeRegs.MCG_C4_value) & (uint8_t)(~(MCG_C4_FCTRIM_MASK | MCG_C4_SCFTRIM_MASK))) | (MCG_C4 & (MCG_C4_FCTRIM_MASK | MCG_C4_SCFTRIM_MASK)); /* Set C4 (FLL output; trim values not changed) */

        MCG_C5 = NextModeRegs.MCG_C5_value; /* Set C5 (PLL settings, PLL reference divider etc.) */

        if (TargetMode & CPU_CLOCK_PLL_MASK) {

          MCG_C5 |= MCG_C5_PLLCLKEN0_MASK;

        }

        MCG_C6 = NextModeRegs.MCG_C6_value; /* Set C6 (PLL select, VCO divider etc.) */

        break;

      case CPU_MCG_MODE_BLPE:

        MCG_C1 = NextModeRegs.MCG_C1_value; /* Set C1 (clock source selection, FLL ext. reference divider, int. reference enable etc.) */

        MCG_C2 = ((NextModeRegs.MCG_C2_value) & (uint8_t)(~(MCG_C2_FCFTRIM_MASK))) | (MCG_C2 & MCG_C2_FCFTRIM_MASK); /* Set C2 (freq. range, ext. and int. reference selection etc.; trim values not changed) */

        OSC_CR = NextModeRegs.OSC_CR_value; /* Set OSC_CR (OSCERCLK enable, oscillator capacitor load) */        

        if (TargetMode & CPU_CLOCK_RTC_OSC_MASK) {

          MCG_C7 = MCG_C7_OSCSEL(1);   /* Select RTC oscillator as MCG clock source */

        } else if (TargetMode & CPU_CLOCK_IRC48M_MASK) {

          MCG_C7 = MCG_C7_OSCSEL(2);   /* Select IRC 48MHz as MCG clock source */

        } else {

          MCG_C7 = 0;                  /* Select system oscillator as MCG clock source */

        }

        if ((TargetMode & CPU_CLOCK_EXTERNAL_CRYSTAL_MASK) != 0) {

          while((MCG_S & MCG_S_OSCINIT0_MASK) == 0x00U) { /* Check that the oscillator is running */

          }

        }

        break;

      case CPU_MCG_MODE_PEE:

      case CPU_MCG_MODE_PBE:

        OSC_CR = NextModeRegs.OSC_CR_value; /* Set OSC_CR (OSCERCLK enable, oscillator capacitor load) */

        if (TargetMode & CPU_CLOCK_RTC_OSC_MASK) {

          MCG_C7 = MCG_C7_OSCSEL(1);   /* Select RTC oscillator as MCG clock source */

        } else if (TargetMode & CPU_CLOCK_IRC48M_MASK) {

          MCG_C7 = MCG_C7_OSCSEL(2);   /* Select IRC 48MHz as MCG clock source */

        } else {

          MCG_C7 = 0;                  /* Select system oscillator as MCG clock source */

        }

        MCG_C1 = NextModeRegs.MCG_C1_value; /* Set C1 (clock source selection, FLL ext. reference divider, int. reference enable etc.) */

        MCG_C2 = ((NextModeRegs.MCG_C2_value) & (uint8_t)(~(MCG_C2_FCFTRIM_MASK))) | (MCG_C2 & MCG_C2_FCFTRIM_MASK); /* Set C2 (freq. range, ext. and int. reference selection etc.; trim values not changed) */

        if ((TargetMode & CPU_MCG_MODE_INDEX_MASK) == CPU_MCG_MODE_PEE) {

          MCG_C5 = CPU_ClockConfigDescriptors[ConfigID].GenRegs.MCG_C5_value; /* Set C5 (PLL settings, PLL reference divider etc.) */

          MCG_C6 = CPU_ClockConfigDescriptors[ConfigID].GenRegs.MCG_C6_value; /* Set C6 (PLL select, VCO divider etc.) */

        } else {

          MCG_C5 = NextModeRegs.MCG_C5_value; /* Set C5 (PLL settings, PLL reference divider etc.) */

          MCG_C6 = NextModeRegs.MCG_C6_value; /* Set C6 (PLL select, VCO divider etc.) */

        }

        while((MCG_S & MCG_S_LOCK0_MASK) == 0x00U) { /* Wait until PLL is locked*/

        }

        break;

      default:

        break;          

    }

    switch (NextMode) {

      case CPU_MCG_MODE_FEI:

      case CPU_MCG_MODE_FEE:

        while((MCG_S & 0x0CU) != 0x00U) { /* Wait until output of the FLL is selected */

        }

        break;

      case CPU_MCG_MODE_FBI:

      case CPU_MCG_MODE_BLPI:

        while((MCG_S & 0x0CU) != 0x04U) { /* Wait until internal reference clock is selected as MCG output */

        }

        break;

      case CPU_MCG_MODE_FBE:

      case CPU_MCG_MODE_BLPE:

      case CPU_MCG_MODE_PBE:

        while((MCG_S & 0x0CU) != 0x08U) { /* Wait until external reference clock is selected as MCG output */

        }

        break;

      case CPU_MCG_MODE_PEE:

        while((MCG_S & 0x0CU) != 0x0CU) { /* Wait until output of the PLL is selected */

        }

        break;

    }

  } while (NextMode != (TargetMode & CPU_MCG_MODE_INDEX_MASK)); /* Loop until the target MCG mode is set */

}

/*

** ===================================================================

**     Method      :  Cpu_SetClockConfiguration (component MK64FN1M0LL12)

*/

/*!

**     @brief

**         Calling of this method will cause the clock configuration

**         change and reconfiguration of all components according to

**         the requested clock configuration setting.

**     @param

**         ModeID          - Clock configuration identifier

**     @return

**                         - ERR_OK - OK.

**                           ERR_RANGE - Mode parameter out of range

*/

/* ===================================================================*/

#if CPU_SET_CLOCK_CONFIGURATION

LDD_TError CPU_SetClockConfiguration(LDD_TClockConfiguration ModeID)

{

  if (ModeID > (CPU_CLOCK_CONFIG_NUMBER - 1U)) {

    return ERR_RANGE;

  }

  if (SMC_PMSTAT == 0x04U) {           /* Test if in VLPR mode */

    /* SMC_PMCTRL: LPWUI=0,RUNM=0,??=0,STOPA=0,STOPM=0 */

    SMC_PMCTRL = (SMC_PMCTRL_RUNM(0x00) | SMC_PMCTRL_STOPM(0x00)); /* Disable very low power mode */

    while((PMC_REGSC & PMC_REGSC_REGONS_MASK) == 0x00U) { /* Wait until the regulator is in run regulation */

    }

    while(SMC_PMSTAT == 0x04U) {       /* Wait until the system is back in RUN mode */

    }

  }

  /* SIM_CLKDIV1: OUTDIV1=0,OUTDIV2=1,OUTDIV3=4,OUTDIV4=4,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */

  SIM_CLKDIV1 = SIM_CLKDIV1_OUTDIV1(0x00) |

                SIM_CLKDIV1_OUTDIV2(0x01) |

                SIM_CLKDIV1_OUTDIV3(0x04) |

                SIM_CLKDIV1_OUTDIV4(0x04); /* Set the system prescalers to safe value */

  switch (ModeID) {

  #if defined(CPU_CLOCK_CONFIG_0)

    case CPU_CLOCK_CONFIG_0:

      CPU_SetClockConfigGenMode(CPU_CLOCK_CONFIG_0);

      break;

  #endif /* defined(CPU_CLOCK_CONFIG_0) */

  #if defined(CPU_CLOCK_CONFIG_1)

    case CPU_CLOCK_CONFIG_1:

      CPU_SetClockConfigGenMode(CPU_CLOCK_CONFIG_1);

      break;

  #endif /* defined(CPU_CLOCK_CONFIG_1) */

  #if defined(CPU_CLOCK_CONFIG_2)

    case CPU_CLOCK_CONFIG_2:

      CPU_SetClockConfigGenMode(CPU_CLOCK_CONFIG_2);

      break;

  #endif /* defined(CPU_CLOCK_CONFIG_2) */

  #if defined(CPU_CLOCK_CONFIG_3)

    case CPU_CLOCK_CONFIG_3:

      CPU_SetClockConfigGenMode(CPU_CLOCK_CONFIG_3);

      break;

  #endif /* defined(CPU_CLOCK_CONFIG_3) */

  #if defined(CPU_CLOCK_CONFIG_4)

    case CPU_CLOCK_CONFIG_4:

      CPU_SetClockConfigGenMode(CPU_CLOCK_CONFIG_4);

      break;

  #endif /* defined(CPU_CLOCK_CONFIG_4) */

  #if defined(CPU_CLOCK_CONFIG_5)

    case CPU_CLOCK_CONFIG_5:

      CPU_SetClockConfigGenMode(CPU_CLOCK_CONFIG_5);

      break;

  #endif /* defined(CPU_CLOCK_CONFIG_5) */

  #if defined(CPU_CLOCK_CONFIG_6)

    case CPU_CLOCK_CONFIG_6:

      CPU_SetClockConfigGenMode(CPU_CLOCK_CONFIG_6);

      break;

  #endif /* defined(CPU_CLOCK_CONFIG_6) */

  #if defined(CPU_CLOCK_CONFIG_7)

    case CPU_CLOCK_CONFIG_7:

      CPU_SetClockConfigGenMode(CPU_CLOCK_CONFIG_7);

      break;

  #endif /* defined(CPU_CLOCK_CONFIG_7) */

    default:

      break;

  }

  SIM_CLKDIV1 = (uint32_t)CPU_ClockConfigDescriptors[ModeID].SysRegs.SIM_CLKDIV1_value; /* Update system prescalers */

  SIM_SOPT1 = (uint32_t)((SIM_SOPT1 & (uint32_t)~(uint32_t)SIM_SOPT1_OSC32KSEL_MASK) | (uint32_t)CPU_ClockConfigDescriptors[ModeID].SysRegs.SIM_SOPT1_value); /* Update 32 kHz oscillator clock source (ERCLK32K) */

  SIM_SOPT2 = (uint32_t)((SIM_SOPT2 & (uint32_t)~(uint32_t)SIM_SOPT2_PLLFLLSEL_MASK) | (uint32_t)CPU_ClockConfigDescriptors[ModeID].SysRegs.SIM_SOPT2_value); /* Update PLL/FLL clock select */

  LDD_SetClockConfiguration(ModeID);   /* Call all LDD components to update the clock configuration */

  ClockConfigurationID = ModeID;       /* Store clock configuration identifier */

  if ((CPU_ClockConfigDescriptors[ClockConfigurationID].PowerMode & CPU_CLOCK_VLP_AUTO_ENABLE_MASK) != 0U) {

    /* SMC_PMCTRL: LPWUI=0,RUNM=2,??=0,STOPA=0,STOPM=0 */

    SMC_PMCTRL = (SMC_PMCTRL_RUNM(0x02) | SMC_PMCTRL_STOPM(0x00)); /* Enable very low power mode */

    if ((CPU_ClockConfigDescriptors[ClockConfigurationID].PowerMode & CPU_CLOCK_VLP_WAKEUP_MASK) != 0U) {

      /* SMC_PMCTRL: LPWUI=1 */

      SMC_PMCTRL |= SMC_PMCTRL_LPWUI_MASK; /* Enable exits to Normal RUN mode on an interrupt */

    }

    while(SMC_PMSTAT != 0x04U) {       /* Wait until in the Very Low Power run mode */

    }

  }

  return ERR_OK;

}

#endif /* CPU_SET_CLOCK_CONFIGURATION */

/*

** ===================================================================

**     Method      :  Cpu_GetClockConfiguration (component MK64FN1M0LL12)

*/

/*!

**     @brief

**         Returns the active clock configuration identifier. The

**         method is automatically enabled if more than one clock

**         configuration is enabled in the component.

**     @return

**                         - Active clock configuration identifier

*/

/* ===================================================================*/

#if CPU_GET_CLOCK_CONFIGURATION

LDD_TClockConfiguration CPU_GetClockConfiguration(void)

{

#if CPU_CLOCK_CONFIG_NUMBER > 1

  return ClockConfigurationID;         /* Return the actual clock configuration identifier */

#else

  return CPU_CLOCK_CONFIG_0;           /* Return the actual clock configuration identifier */

#endif

}

#endif /* CPU_GET_CLOCK_CONFIGURATION */

/*

** ===================================================================

**     Method      :  Cpu_SetOperationMode (component MK64FN1M0LL12)

*/

/*!

**     @brief

**         This method requests to change the component's operation

**         mode (RUN, WAIT, SLEEP, STOP). The target operation mode

**         will be entered immediately.

**         See [Operation mode settings] for further details of the

**         operation modes mapping to low power modes of the cpu.

**     @param

**         OperationMode   - Requested driver

**                           operation mode

**     @param

**         ModeChangeCallback - Callback to

**                           notify the upper layer once a mode has been

**                           changed. Parameter is ignored, only for

**                           compatibility of API with other components.

**     @param

**         ModeChangeCallbackParamPtr

**                           - Pointer to callback parameter to notify

**                           the upper layer once a mode has been

**                           changed. Parameter is ignored, only for

**                           compatibility of API with other components.

**     @return

**                         - Error code

**                           ERR_OK - OK

**                           ERR_PARAM_MODE - Invalid operation mode

*/

/* ===================================================================*/

#if CPU_SET_OPERATION_MODE

LDD_TError CPU_SetOperationMode(LDD_TDriverOperationMode OperationMode, LDD_TCallback ModeChangeCallback, LDD_TCallbackParam *ModeChangeCallbackParamPtr)

{

  (void) ModeChangeCallback;           /* Parameter is not used, suppress unused argument warning */

  (void) ModeChangeCallbackParamPtr;   /* Parameter is not used, suppress unused argument warning */

    switch (OperationMode) {

    case DOM_RUN:

      /* SCB_SCR: SLEEPDEEP=0,SLEEPONEXIT=0 */

      SCB_SCR &= (uint32_t)~(uint32_t)(

                  SCB_SCR_SLEEPDEEP_MASK |

                  SCB_SCR_SLEEPONEXIT_MASK

                 );                    /* Set RUN or VLPR mode */

      if ((CPU_ClockConfigDescriptors[ClockConfigurationID].Mode & CPU_MCG_MODE_INDEX_MASK) == CPU_MCG_MODE_PEE) {

        if ((MCG_S & MCG_S_CLKST_MASK) != MCG_S_CLKST(3)) { /* If in PBE mode, switch to PEE. PEE to PBE transition was caused by wakeup from low power mode. */

          /* MCG_C1: CLKS=0,IREFS=0 */

          MCG_C1 &= (uint8_t)~(uint8_t)((MCG_C1_CLKS(0x03) | MCG_C1_IREFS_MASK)); /* Switch back to the PEE mode */

          while( (MCG_S & MCG_S_LOCK0_MASK) == 0x00U) { /* Wait for PLL lock */

          }

        }

      }

      break;

    case DOM_WAIT:

      /* SCB_SCR: SLEEPDEEP=0 */

      SCB_SCR &= (uint32_t)~(uint32_t)(SCB_SCR_SLEEPDEEP_MASK); /* WAIT or VLPW mode can be entered after WFI instruction call */

  #if CPU_LOW_POWER_WAIT_SLEEP_ON_EXIT

      /* SCB_SCR: SLEEPONEXIT=1 */

      SCB_SCR |= SCB_SCR_SLEEPONEXIT_MASK; /* Enter wait state on ISR exit */

  #else /* CPU_LOW_POWER_WAIT_SLEEP_ON_EXIT */

      /* SCB_SCR: SLEEPONEXIT=0 */

      SCB_SCR &= (uint32_t)~(uint32_t)(SCB_SCR_SLEEPONEXIT_MASK); /* Do not enter wait state on ISR exit */

  #endif /* CPU_LOW_POWER_WAIT_SLEEP_ON_EXIT */

      PE_WFI();                        /* Enter WAIT or VLPW state */

      break;

    case DOM_SLEEP:

      /* SCB_SCR: SLEEPDEEP=1 */

      SCB_SCR |= SCB_SCR_SLEEPDEEP_MASK; /* STOP VLPS or VLLSx mode can be entered after WFI instruction call */

      /* SMC_PMCTRL: STOPM=0 */

      SMC_PMCTRL &= (uint8_t)~(uint8_t)(SMC_PMCTRL_STOPM(0x07)); /* Set normal STOP mode */

      (void)(SMC_PMCTRL == 0U);        /* Dummy read of SMC_PMCTRL to ensure the register is written before entering low power mode */

  #if CPU_LOW_POWER_SLEEP_SLEEP_ON_EXIT

      /* SCB_SCR: SLEEPONEXIT=1 */

      SCB_SCR |= SCB_SCR_SLEEPONEXIT_MASK; /* Enter stop state on ISR exit */

  #else /* CPU_LOW_POWER_SLEEP_SLEEP_ON_EXIT */

      /* SCB_SCR: SLEEPONEXIT=0 */

      SCB_SCR &= (uint32_t)~(uint32_t)(SCB_SCR_SLEEPONEXIT_MASK); /* Do not enter stop state on ISR exit */

  #endif /* CPU_LOW_POWER_SLEEP_SLEEP_ON_EXIT */

      PE_WFI();                        /* Enter STOP state */

      break;

    case DOM_STOP:

  #if CPU_LOW_POWER_STOP

      /* Clear LLWU flags */

      /* LLWU_F1: WUF7=1,WUF6=1,WUF5=1,WUF4=1,WUF3=1,WUF2=1,WUF1=1,WUF0=1 */

      LLWU_F1 = LLWU_F1_WUF7_MASK |

                LLWU_F1_WUF6_MASK |

                LLWU_F1_WUF5_MASK |

                LLWU_F1_WUF4_MASK |

                LLWU_F1_WUF3_MASK |

                LLWU_F1_WUF2_MASK |

                LLWU_F1_WUF1_MASK |

                LLWU_F1_WUF0_MASK;

      /* LLWU_F2: WUF15=1,WUF14=1,WUF13=1,WUF12=1,WUF11=1,WUF10=1,WUF9=1,WUF8=1 */

      LLWU_F2 = LLWU_F2_WUF15_MASK |

                LLWU_F2_WUF14_MASK |

                LLWU_F2_WUF13_MASK |

                LLWU_F2_WUF12_MASK |

                LLWU_F2_WUF11_MASK |

                LLWU_F2_WUF10_MASK |

                LLWU_F2_WUF9_MASK |

                LLWU_F2_WUF8_MASK;

      /* LLWU_F3: MWUF7=1,MWUF6=1,MWUF5=1,MWUF4=1,MWUF3=1,MWUF2=1,MWUF1=1,MWUF0=1 */

      LLWU_F3 = LLWU_F3_MWUF7_MASK |

                LLWU_F3_MWUF6_MASK |

                LLWU_F3_MWUF5_MASK |

                LLWU_F3_MWUF4_MASK |

                LLWU_F3_MWUF3_MASK |

                LLWU_F3_MWUF2_MASK |

                LLWU_F3_MWUF1_MASK |

                LLWU_F3_MWUF0_MASK;

      /* LLWU_FILT1: FILTF=1 */

      LLWU_FILT1 |= LLWU_FILT1_FILTF_MASK;

      /* LLWU_FILT2: FILTF=1 */

      LLWU_FILT2 |= LLWU_FILT2_FILTF_MASK;

      /* SCB_SCR: SLEEPONEXIT=0 */

      SCB_SCR &= (uint32_t)~(uint32_t)(SCB_SCR_SLEEPONEXIT_MASK); /* Do not enter stop state on ISR exit */

      /* SCB_SCR: SLEEPDEEP=1 */

      SCB_SCR |= SCB_SCR_SLEEPDEEP_MASK; /* STOP VLPS or VLLSx mode can be entered after WFI instruction call */

    #if (CPU_LOW_POWER_STOP == CPU_LOW_POWER_STOP_LLS)

      /* SMC_PMCTRL: STOPM=3 */

      SMC_PMCTRL = (uint8_t)((SMC_PMCTRL & (uint8_t)~(uint8_t)(

                    SMC_PMCTRL_STOPM(0x04)

                   )) | (uint8_t)(

                    SMC_PMCTRL_STOPM(0x03)

                   ));                 /* Set Very-low-leakage mode */

    #else

      /* SMC_PMCTRL: STOPM=4 */

      SMC_PMCTRL = (uint8_t)((SMC_PMCTRL & (uint8_t)~(uint8_t)(

                    SMC_PMCTRL_STOPM(0x03)

                   )) | (uint8_t)(

                    SMC_PMCTRL_STOPM(0x04)

                   ));                 /* Set Very-low-leakage mode */

      #if (CPU_LOW_POWER_STOP == CPU_LOW_POWER_STOP_VLLS0)

        #if (CPU_LOW_POWER_STOP_POR_DETECT)

      /* SMC_VLLSCTRL: ??=0,??=0,PORPO=0,??=0,??=0,VLLSM=0 */

      SMC_VLLSCTRL = SMC_VLLSCTRL_VLLSM(0x00); /* Set VLLS0 mode with POR detect enabled */

        #else /* CPU_LOW_POWER_STOP_POR_DETECT */

      /* SMC_VLLSCTRL: ??=0,??=0,PORPO=1,??=0,??=0,VLLSM=0 */

      SMC_VLLSCTRL = (SMC_VLLSCTRL_PORPO_MASK | SMC_VLLSCTRL_VLLSM(0x00)); /* Set VLLS0 mode with POR detect disabled */

        #endif /* CPU_LOW_POWER_STOP_POR_DETECT */

      #elif (CPU_LOW_POWER_STOP == CPU_LOW_POWER_STOP_VLLS3)

      /* SMC_VLLSCTRL: ??=0,??=0,PORPO=0,??=0,??=0,VLLSM=3 */

      SMC_VLLSCTRL = SMC_VLLSCTRL_VLLSM(0x03); /* Set VLLS3 mode */

      #elif (CPU_LOW_POWER_STOP == CPU_LOW_POWER_STOP_VLLS2)

      /* SMC_VLLSCTRL: ??=0,??=0,PORPO=0,??=0,??=0,VLLSM=2 */

      SMC_VLLSCTRL = SMC_VLLSCTRL_VLLSM(0x02); /* Set VLLS2 mode */

      #elif (CPU_LOW_POWER_STOP == CPU_LOW_POWER_STOP_VLLS1)

      /* SMC_VLLSCTRL: ??=0,??=0,PORPO=0,??=0,??=0,VLLSM=1 */

      SMC_VLLSCTRL = SMC_VLLSCTRL_VLLSM(0x01); /* Set VLLS1 mode */

      #else /* CPU_LOW_POWER_STOP == CPU_LOW_POWER_STOP_VLLS3 */

            #error Unsupported STOP low power mode

      #endif /* CPU_LOW_POWER_STOP == CPU_LOW_POWER_STOP_VLLS3 */

    #endif /* CPU_LOW_POWER_STOP == CPU_LOW_POWER_STOP_LLS */

      (void)(SMC_PMCTRL == 0U);        /* Dummy read of SMC_PMCTRL to ensure the register is written before entering low power mode */

      PE_WFI();                        /* Enter STOP state */

  #endif /* CPU_LOW_POWER_STOP */

      break;

    default:

      return ERR_PARAM_MODE;

  }

  return ERR_OK;

}

#endif /* CPU_SET_OPERATION_MODE */

/*

** ===================================================================

**     Method      :  Cpu_EnableInt (component MK64FN1M0LL12)

*/

/*!

**     @brief

**         Enables all maskable interrupts.

*/

/* ===================================================================*/

#if CPU_ENABLE_INT

void CPU_EnableInt(void)

{

__EI();

}

#endif /* CPU_ENABLE_INT */

/*

** ===================================================================

**     Method      :  Cpu_DisableInt (component MK64FN1M0LL12)

*/

/*!

**     @brief

**         Disables all maskable interrupts.

*/

/* ===================================================================*/

#if CPU_DISABLE_INT

void CPU_DisableInt(void)

{

__DI();

}

#endif /* CPU_DISABLE_INT */

/*

** ===================================================================

**     Method      :  Cpu_MCGAutoTrim (component MK64FN1M0LL12)

*/

/*!

**     @brief

**         This method uses MCG auto trim feature to trim internal

**         reference clock. This method can be used only in a clock

**         configuration which derives its bus clock from external

**         reference clock ([MCG mode] must be one of the following

**         modes - FEE, FBE, BLPE, PEE, PBE) and if value of [Bus clock]

**         is in the range <8; 16>MHz.

**         The slow internal reference clock is trimmed to the value

**         selected by [Slow internal reference clock [kHz]] property.

**         The fast internal reference clock will be trimmed to value

**         4MHz.

**     @param

**         ClockSelect     - Selects which internal

**                           reference clock will be trimmed.

**                           0 ... slow (32kHz) internal reference clock

**                           will be trimmed

**                           > 0 ... fast (4MHz) internal reference

**                           clock will be trimmed

**     @return

**                         - Error code

**                           ERR_OK - OK

**                           ERR_SPEED - The method does not work in the

**                           active clock configuration.

**                           ERR_FAILED - Autotrim process failed.

*/

/* ===================================================================*/

#if CPU_MCG_AUTO_TRIM

LDD_TError CPU_MCGAutoTrim(uint8_t ClockSelect)

{

  uint16_t CompareValue;               /* Autotrim compare value expected count */

  uint16_t BusClockMHz = (uint16_t)((uint32_t)(CPU_ClockConfigDescriptors[ClockConfigurationID].BusClock) /1000000UL); /* Bus clock in MHz */

  /* Calculate compare value */

  if (((CPU_ClockConfigDescriptors[ClockConfigurationID].Mode & (CPU_CLOCK_EXTERNAL_CLOCK_MASK | CPU_CLOCK_EXTERNAL_CRYSTAL_MASK)) != 0) && (BusClockMHz >= 8U) && (BusClockMHz <= 16U)) {

    if (ClockSelect == 0x00U) {

      CompareValue = (uint16_t)(21000 * BusClockMHz / CPU_INT_SLOW_CLK_HZ); /* Slow internal reference clock */

    } else {

      CompareValue = (uint16_t)(672U * BusClockMHz); /* Fast internal reference clock */

    }

  } else {

    return ERR_SPEED;                  /* MCU has to be clocked from external clock and has to have bus clock in allowed range */

  }

  MCG_ATCVH = (uint8_t)(CompareValue >> 8U); /* Set compare value high half */

  MCG_ATCVL = (uint8_t)(CompareValue & 255U); /* Set compare value low half */

  if (ClockSelect == 0x00U) {

    /* MCG_SC: ATME=1,ATMS=0,LOCS0=0 */

    MCG_SC = (uint8_t)((MCG_SC & (uint8_t)~(uint8_t)(

              MCG_SC_ATMS_MASK |

              MCG_SC_LOCS0_MASK

             )) | (uint8_t)(

              MCG_SC_ATME_MASK

             ));                       /* Start trimming of the slow internal reference clock */

  } else {

    /* MCG_SC: ATME=1,ATMS=1,LOCS0=0 */

    MCG_SC = (uint8_t)((MCG_SC & (uint8_t)~(uint8_t)(

              MCG_SC_LOCS0_MASK

             )) | (uint8_t)(

              MCG_SC_ATME_MASK |

              MCG_SC_ATMS_MASK

             ));                       /* Start trimming of the fast internal reference clock */

  }

  while ((MCG_SC & MCG_SC_ATME_MASK) != 0x00U) { /* Wait until autotrim completes */

  }

  if ((MCG_SC & MCG_SC_ATMF_MASK) == 0x00U) {

    return ERR_OK;                     /* Trim operation completed successfully */

  } else {

    return ERR_FAILED;                 /* Trim operation failed */

  }

}

#endif /* CPU_MCG_AUTO_TRIM */

/*

** ===================================================================

**     Method      :  Cpu_VLPModeEnable (component MK64FN1M0LL12)

*/

/*!

**     @brief

**         This method enables Very Low Power (VLP) mode in the active

**         clock configuration. To enable the VLP mode the active clock

**         configuration has to have the [Very low power mode] property

**         enabled. The method waits until the entry to the VLP mode is

**         confirmed by a power management module status register.

**         This method can be enabled only when one of the clock

**         configurations modes have the [Very low power mode] property

**         enabled.

**     @return

**                         - Error code

**                           ERR_OK - OK

**                           ERR_SPEED - the Very Low Power mode is not

**                           supported in the active clock configuration.

*/

/* ===================================================================*/

#if CPU_VLP_MODE_ENABLE

LDD_TError CPU_VLPModeEnable(void)

{

  if ((CPU_ClockConfigDescriptors[ClockConfigurationID].PowerMode & CPU_CLOCK_VLP_ENABLE_MASK) == 0U) {

    return ERR_SPEED;                  /* Very low power mode not enabled in the active clock configuration. */

  }

  if (SMC_PMSTAT == 0x04U) {           /* If the system is already in VLP mode, return */

    return ERR_OK;

  }

  /* SMC_PMCTRL: LPWUI=0,RUNM=2,??=0,STOPA=0,STOPM=0 */

  SMC_PMCTRL = (SMC_PMCTRL_RUNM(0x02) | SMC_PMCTRL_STOPM(0x00)); /* Enable very low power mode */

  if ((CPU_ClockConfigDescriptors[ClockConfigurationID].PowerMode & CPU_CLOCK_VLP_WAKEUP_MASK) == 0U) {

    /* SMC_PMCTRL: LPWUI=1 */

    SMC_PMCTRL |= SMC_PMCTRL_LPWUI_MASK; /* Enable exits to Normal RUN mode on an interrupt */

  }

  while(SMC_PMSTAT != 0x04U) {         /* Wait until in the Very Low Power run mode */

  }

  return ERR_OK;

}

#endif /* CPU_VLP_MODE_ENABLE */

/*

** ===================================================================

**     Method      :  Cpu_VLPModeDisable (component MK64FN1M0LL12)

*/

/*!

**     @brief

**         This method disables the Very Low Power (VLP) mode in the

**         active clock configuration. The method waits until the exit

**         of the VLP mode is confirmed by a power management module

**         status register.

**         This method can be enabled only when one of the clock

**         configurations have the [Very low power mode] property

**         enabled.

**     @return

**                         - Error code

**                           ERR_OK - OK

**                           ERR_SPEED - the Very Low Power mode is not

**                           supported in the active clock configuration.

*/

/* ===================================================================*/

#if CPU_VLP_MODE_DISABLE

LDD_TError CPU_VLPModeDisable(void)

{

  if ((CPU_ClockConfigDescriptors[ClockConfigurationID].PowerMode & CPU_CLOCK_VLP_ENABLE_MASK) == 0U) {

    return ERR_SPEED;                  /* Very low power mode not enabled in the active clock configuration. */

  }

  if (SMC_PMSTAT == 0x04U) {           /* Test if in VLPR mode */

    /* SMC_PMCTRL: LPWUI=0,RUNM=0,??=0,STOPA=0,STOPM=0 */

    SMC_PMCTRL = (SMC_PMCTRL_RUNM(0x00) | SMC_PMCTRL_STOPM(0x00)); /* Disable very low power mode */

    while((PMC_REGSC & PMC_REGSC_REGONS_MASK) == 0x00U) { /* Wait until the regulator is in run regulation */

    }

    while(SMC_PMSTAT == 0x04U) {       /* Wait until the system is back in RUN mode */

    }

  }

  return ERR_OK;

}

#endif /* CPU_VLP_MODE_DISABLE */

/*

** ===================================================================

**     Method      :  Cpu_SystemReset (component MK64FN1M0LL12)

*/

/*!

**     @brief

**         This method initiates a system reset request to reset the

**         CPU.

*/

/* ===================================================================*/

#if CPU_SYSTEM_RESET

void CPU_SystemReset(void)

{

  /* SCB_AIRCR: VECTKEY=0x05FA,SYSRESETREQ=1 */

  SCB_AIRCR = (uint32_t)((SCB_AIRCR & (uint32_t)~(uint32_t)(

               SCB_AIRCR_VECTKEY(0xFA05)

              )) | (uint32_t)(

               SCB_AIRCR_VECTKEY(0x05FA) |

               SCB_AIRCR_SYSRESETREQ_MASK

              ));                      /* Request system reset */

  while(1) {                           /* Wait until reset */

  }

}

#endif /* CPU_SYSTEM_RESET */

#ifdef __cplusplus

}

#endif

/* END CPU_Init.c */

/*!

** @}

*/

/*

** ###################################################################

**

**     This file is a part of Processor Expert static initialization

**     library for the Freescale Kinetis series of microcontrollers.

**

** ###################################################################

*/

Erich

0 项奖励
回复