Cutting traceD0 and tracdD1 (PA10 & PA9) on Tower to control MII Ethernet. Problems?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cutting traceD0 and tracdD1 (PA10 & PA9) on Tower to control MII Ethernet. Problems?

ソリューションへジャンプ
668件の閲覧回数
cavebiker
Contributor V

Has anyone done this? and are there any issues?

I'm using a PEmicro Multilink Universal with a 20 pin connector to Jtag on a K70 tower System (I think is the same for any Kx Tower System)

I plan to just cut these 2 traces to the Jtag so I can use them to talk to a KSZ8051MNL MII-PHY. Fingers crossed.

Thanks for the look

Cheers,

Tom

タグ(3)
0 件の賞賛
返信
1 解決策
547件の閲覧回数
cavebiker
Contributor V

This seems to be working fine :smileyhappy:

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
548件の閲覧回数
cavebiker
Contributor V

This seems to be working fine :smileyhappy:

0 件の賞賛
返信