Configure DMA for DAC with Processor Expert | |
Description: | I have tried to configure CW10.1 using processor expert to transfer by DMA to the DAC..... I have two data buffers, one is being DMA'd out to the DAC at a specified rate, while the other is being filled, once the buffer being transferred is done, it switches to the other one. Its an audio application I am sending data to DAC at 32Khz..... So I would think I could use PIT or similar to trigger the DMA transfers..... Can you walk me through the setup? Send me demo code already doing this? I have K60 Tower kit and CW10.1 fully updated. Thanks. |
This was posted on my support page and has not been looked at for 5 days from FREESCALE :smileysad:
Hope someone can help.
Hello,
you can find an example related to the DMA transfers on "Typical Usage" page in help of DAC_LDD component, the help is available through "Help" menu command from component´s pop-up menu.
Note:
You can also find a basic example project of using DAC_LDD and ADC_LDD in the following folder:
{CodeWarrior}\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\TWR-K40X256\DAC_ADC\
best regards
Vojtech Filip
Processor Expert Support Team
Hello,
could you please post here some simple demonstration project of your problem?
best regards
Vojtech Filip
Processor Expert Support Team
Hello,
I think this issue was already solved within this thread:
https://community.freescale.com/message/97760#97760
Am I corect?
best regards
Vojtech Filip
Processor Expert Support Team
I can get buffer to buffer DMA to happen, just declare 2 buffers in memory and move one to another..... BUT I can not get one memory buffer to go to the DAC, I will look at the examples you sent, the ones they give for examples in the CW help files do not help.
Thanks.