Assert RSTD will clear DTW bit field

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Assert RSTD will clear DTW bit field

2,288件の閲覧回数
tsi-chung_liew
NXP Employee
NXP Employee

pdrake‌

Question:

System control register.
RSTD in the SYS CTRL register (PROCTL) - it’s not clearly documented that DTW bit gets cleared when this is asserted.

Answer:

The following registers and bits are cleared by RSTD
• Data Port register
• Buffer is cleared and initialized.
• Present State register
• Buffer Read Enable
• Buffer Write Enable
• Read Transfer Active
• Write Transfer Active
• DATA Line Active
• Command Inhibit (DATA) Protocol Control register
• Continue Request
• Stop At Block Gap Request Interrupt Status register
• Buffer Read Ready
• Buffer Write Ready
• DMA Interrupt
• Block Gap Event
• Transfer Complete

Setting SYS_CTRL[RSTD] will clear all the registers mentioned in the RSTD field description. DTW field will be clear if set, DTW is considering as PROT_Command Inhibit (DATA) Protocol Control Registers.

0 件の賞賛
返信
2 返答(返信)

2,160件の閲覧回数
davidsidrane
Contributor I

Hi Tc an Phlip,

This is still incorrect, incomplete and unclear:

The following registers and bits are cleared by RSTD
• Data Port register
• Buffer is cleared and initialized.
• Present State register
• Buffer Read Enable
• Buffer Write Enable
• Read Transfer Active
• Write Transfer Active
• DATA Line Active
• Command Inhibit (DATA) Protocol Control register
• Continue Request
• Stop At Block Gap Request Interrupt Status register
• Buffer Read Ready
• Buffer Write Ready
• DMA Interrupt
• Block Gap Event
• Transfer Complete

There are 1) formatting errors, 2) ambiguous names, and 3) not all bit are cleared in all registers.

1) Formatting:

The following registers and bits are cleared by RSTD
• Data Port register
• Buffer is cleared and initialized.
• Present State register
• Buffer Read Enable
• Buffer Write Enable
• Read Transfer Active
• Write Transfer Active
• DATA Line Active
• Command Inhibit (DATA) MISSING NEW LINE Protocol Control register
• Continue Request
• Stop At Block Gap Request MISSING NEW LINE Interrupt Status register
• Buffer Read Ready
• Buffer Write Ready
• DMA Interrupt
• Block Gap Event
• Transfer Complete

 

2) Search the manual for each of the above names. You will be frustrated to only find them in ONLY the one table.

 Using register names that result in unambiguous search results in the manual would be super helpful

like SDHC_SYSCTL or the full name and Buffer Data Port register or better yet SDHC_DATPORT

3) Not all the bits in all the registers are cleared. The test is simple: a) set all the non-reserved bits in SDHC_PROCTL b) assert  SDHC_SYSCTL[RSTD] and c) read the results of  SDHC_PROCTL.

The point I would like to reinforce, is that the documentation can only add value for the end user if it is an unambiguous reference. 

If I had described the test above as: do the reset and read the register. Would that be clear? What reset? System reset POR on reset or SDHC_SYSCTL[RSTD]? 

David

0 件の賞賛
返信

2,160件の閲覧回数
davidsidrane
Contributor I

The above is in reference to 

K66 Sub-Family Reference Manual
Supports: MK66FN2M0VMD18, MK66FX1M0VMD18,
MK66FN2M0VLQ18, MK66FX1M0VLQ18,
Document Number: K66P144M180SF5RMV2
Rev. 2, May 2015

0 件の賞賛
返信