Are digital K60 I/O 5V tolerant when used as inputs?
In the datasheet the Absolute Maximum Rating is -0.3V to +5.5V, so it seems it would be safe to interface a 5V signal.
What do you think?
I think that's fine, but I haven't actually tried it myself.
Anyone from Freescale can confirm?
Does anyone know if the ADC inputs on the Kinetis 40 series are 5V tolerant? The data says the digital I/Os only, not the analog inputs are 5V tolerant. The definition of analog is unclear - some of the ADC inputs have digital input options too.