I am using KDS v3.0.0 and have been using PE a lot for all the peripherals on a K65 uC. I find sometimes that when I change a setting a save it that it doesn't always rebuild. I found changing the baud rate in my UART component especially prone to this. Is there a way to force KDS to tell PE that something changed and have it rebuild so that the changes are reflected in the Generated_Code?
Thank you,
Kevin
Hi Kevin,
I have not seen something like this.
if you change a setting, and you generate code, and it does not build the changed files, then this would be a bug.
Could you report other details? Have you generated code?
Note that there is a setting to disable code generation (see How to Avoid Slow Processor Expert Projects | MCU on Eclipse ) in case you want to do it manually. Maybe you have enabled that setting, and code is not generated after you have changed something?
Thanks,
Erich
Hello Kevin,
After you change the code , if you do not want the PE change the code you write , you can select ""Don't Write Generated Component Modules"
thus , when rebuild the project , the code you write won't disappeared .
Hope it helps
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Have a great day,
Alice