Support of K26 and K66 in KDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Support of K26 and K66 in KDS

862 Views
lustfulrat
Contributor I

Hello,

 

Recently I've got some samples of K26 and K66 from Freescale (I'd like to try and test 180MHz clocking) but it looks that these devices are not supported by KDS. I have KDS 3.0.0 with all recent updates on 64bit Ubuntu and K22 and K26 are not visible in Devices list in Project wizard. Am I miss something? Maybe I should install some "special" update or package?

 

If these processors are really not supported by KDS which IDE should I use to handle it?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

571 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello lus,

Dose this can meet your requirement?

pastedImage_0.png

If yes , please install KSDK1.2 , you can download it here :

Software Development Kit for Kinetis MCUs|Freescale

then please refer to this to install the update on KDS (especial the "5 Run a demo using Kinetis Design Studio IDE")

http://cache.freescale.com/files/soft_dev_tools/doc/support_info/KSDK12GSUG.pdf?fsrch=1

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply