Processor Expert - Build tries to create files in C:/Freescale/KDS_1.1.1 folder

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert - Build tries to create files in C:/Freescale/KDS_1.1.1 folder

Jump to solution
848 Views
johnbaker
Contributor IV

I was trying to create a project using Processor Expert.  I created a new KDS workspace.  When creating the project I selected the 'Stand alone' option.  Why, when I try to build the project is it trying save PE generated code files in the KDS home folder instead of in my project folder in my workspace? (See attached snapshot).

 

Thanks,

 

John Baker

Labels (1)
0 Kudos
Reply
1 Solution
698 Views
BlackNight
NXP Employee
NXP Employee

It asks you to create (or copy from) the files on the left to the location on the right.

So the source of the file is in c:\freescale\kds_1.1.1/eclipse...... to your project subfolder Generated_Code/....

It should create the files inside your project structure, not in KDS.

Erich

View solution in original post

0 Kudos
Reply
3 Replies
699 Views
BlackNight
NXP Employee
NXP Employee

It asks you to create (or copy from) the files on the left to the location on the right.

So the source of the file is in c:\freescale\kds_1.1.1/eclipse...... to your project subfolder Generated_Code/....

It should create the files inside your project structure, not in KDS.

Erich

0 Kudos
Reply
698 Views
johnbaker
Contributor IV

Thank Erich,    I guess I was just overly cautious.

John

0 Kudos
Reply
698 Views
johnbaker
Contributor IV

When I look at the Properties -> Processor Expert -> Generated code directory:  it points to 'Generated_Code' as it should.  (see attached snapshot)

Thanks,

John

0 Kudos
Reply