KDS Kinetis Bootloader (KBOOT) Support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KDS Kinetis Bootloader (KBOOT) Support

跳至解决方案
2,744 次查看
ramstell
Contributor III

The current version of the Bootloader V1.1.0 seems to only support the IAR Toolchain.

 

Are there plans to add support for Kinetis Design Studio?

 

Kind regards

Roger

标签 (1)
1 解答
1,941 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Roger,

The Kinetis Bootloader v 1.2.0 will support KDS and is planned to be released next week.

Once it is available you can download it from this page:

Kinetis Bootloader|Freescale

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
14 回复数
1,941 次查看
a8Chcx
Contributor V

Thanks, Guys.

It works fine now...

0 项奖励
回复
1,941 次查看
a8Chcx
Contributor V

Hi Iva,

I am using KDS 3.0.0 and KSDK 1.2.0 to build FREEDOM K64F Bootloader and found the problem, see attached doc.

Please let me know where the problem can be?

Thanks,

Christie

0 项奖励
回复
1,941 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Cristie,

Those errors happen because the project was imported to the workspace with the "Copy projects into workspace" enabled, when you only import the example project to your workspace, then you are leaving the project in its original location in the file system and the links are still valid, but when you "copy" the project to the workspace, only the project folder is copied and not the linked files/resources causing those errors when compiling.

In order to fix the problems you need to delete that project from your workspace and import the example again but this time make sure the "Copy projects into workspace" is not selected:

pastedImage_2.png

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 项奖励
回复
1,941 次查看
a8Chcx
Contributor V

Hi Gorge/Carlos,

I am using bootloader for FREEDOM K64F project to generate the *.elf and works fine.

Then I use P&E "Debug" to load it into my board, nothing wrong.

But, when I run it, nothing displayed on HyperTerminal. I am using PTB16/PTB17 as my UART port. In this project it says PTA14/15 in bootloader_config.h that I think is wrong.

Could you tell me there is any way to see it is running on UART0? I confirmed that my UART0 is working fine by using another project?

Thanks,

Christie

0 项奖励
回复
1,941 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Cristie,

I would recommend you to create a new post for this question on the Kinetis Microcontrollers​ community.

Best Regards!

Carlos Mendoza

Technical Support Engineer

0 项奖励
回复
1,941 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Christie:

Remove the project from the workspace and import it again but DO NOT select "Copy projects into workspace":

pastedImage_0.png

The source and header files are "linked" to the project. If you copy the project then the links are broken.

Regards!

Jorge Gonzalez

0 项奖励
回复
1,941 次查看
a8Chcx
Contributor V

Hi Iva,

I am using MK64FN1M0VLL12 MCU that is the same as FREEDOM K64F platform.

Can I make both development environments available?

Thanks,

Christie

0 项奖励
回复
1,942 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Roger,

The Kinetis Bootloader v 1.2.0 will support KDS and is planned to be released next week.

Once it is available you can download it from this page:

Kinetis Bootloader|Freescale

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,941 次查看
a8Chcx
Contributor V

Hi Carlos,

This boot-loader is released? Where can I download it for my K64F?

Thanks,

Christie

0 项奖励
回复
1,941 次查看
DavidS
NXP Employee
NXP Employee

Slight update to release....sorry for delay.

Original date was last week. But we have been fixing a pinmux issue and adding some ease-of-use feature. ETA would be early next week.

Regards,

David

1,941 次查看
gierdo
Contributor I

Hi!

Are there any news concerning the release of kboot 1.2.0?

Thanks for your info!

0 项奖励
回复
1,941 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Dominikus Gierlach,

KBOOT 1.2 we expect in these days, no later than by the end of the week.

I hope this helps,

Iva

0 项奖励
回复
1,941 次查看
a8Chcx
Contributor V

Hi Iva,

The version 1.2 is released. Thank you. I have the following question:

I am using KDS 2.0.0 and KSDK 1.1.0 now.

Do I have to use KDS 3.0.0 and KSDK 1.2.0?

Can I make both development available on the same machine?

Thanks,

Christie

0 项奖励
回复
1,941 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Christie Su,

Yes, it is better to use these newest versions.

When you have project developed in KSDK 1.1.0 you should migrate your project to KSDK 1.2 because structure changes greatly.

please what device are you using?

Regards!

Iva

0 项奖励
回复