Just updated from KDS 3.0.0 to 3.1.0 and now I can not work.
The KDS is too slow.
The Windows Task Manager show the KDS using about 20% of CPU..
Anyone has a clue on what is wrong?
Hi,
I have KDS3.1.0 installed, it doesn't slow slow down my KDS.
there are several possibles reasons that may slow KDS:
- there might be some other SWs installed slowing down KDS, please turn off virus defender and firewall to see how it works.
- compiler may take time search for files in too many places, please check path setting if you include all path well. you may create a simple new project with wizard, see how this new project work.
- see if this thread can help you:
Very very slow build with KDS on some Windows computers
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you Jennie Zhang.
Yeah, maybe there is some process running on my Windows that make the KDS impossible to use, but I could not figure which.
I had to desinstall the update and back to KDS 3.0.0.
Have a nice weekend
You are welcome!
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------