Hi,
I wanted to create a project in kds and run KEA-128 demo UART code given by NXP but it is showing me error in makefile.
I have attached the project and the screen shot of the error also.
How to fix this?
Original Attachment has been moved to: kds_KEA-128_uart_example.zip
Hello ,
First ,your code have error , the register of UART_S1 is a read-only status flags,
can not write :
while on your code :
Hope it helps
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello VIGNESH,
About your project, there is so much problem , first have not initialize the UART.
For quickly solve your problem , i make a UART2 demo on TRK-KEA128 board on KDS.
The bound rate is 115200 , you can check it .
Hope it helps
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
How to add things in the include path?
How to change the build variables?
what is rt library?
Hello,
Could you please take a screenshot what do you mentioned ?
BR
Alice
Hello VIGNESH,
I do not recommend you use the porting , for we don't know this doc is for which version
of KDS, different version use different tools ,and porting is bother .
I recommend you create one new project on kds, then copy the application code into that project .
Hope it helps
Alice
Hi Alice,
Ya sure, I willthe start with a new kds project :smileyhappy:.