The S32K1xx chip can be connected using freemaster without any configuration. How can I disable this connection?
Hi @LIZQ,
Are you using PD-BDM (Packet Driven BDM) communication plugin ?
If so - you can disable it by updating the following definition in the embedded application (freemaster_cfg.h
#define FMSTR_DISABLE 1 /* To disable all FreeMASTER functionalities */
Note: FreeMASTER will still be able to connect to the board via standard BDM plugin to read and write target memory over debug interface. This plugin relies entirely on the J-Link Probe and on-target BDM/JTAG module and does not require FreeMASTER specific enablement.
The topic you want to address (disable/secure debug interface) is not related to FreeMASTER.
You may want to check CSEc (Cryptographic Service Engine compressed) Security Module first.
More information/details can be addressed on S32K144 product community space.