FreeMASTER source codes

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FreeMASTER source codes

跳至解决方案
3,290 次查看
stepan_podhorsk
Contributor II

Hello,

please can anybody tell me whether the source codes for the FreeMASTER software are available for download? Thanks.

标记 (2)
0 项奖励
回复
1 解答
3,185 次查看
MichalH
NXP Apps Support
NXP Apps Support

Dear Stepan,

the source code of FreeMASTER serial and CAN communication driver is available in the MCUXpresso SDK. The source code is the same for all MCUs supported by the SDK, so just pick any of the supported devices or boards (e.g. FRDM-K64F) and add the FreeMASTER  middleware component. The sources will be located in middleware/freemaster directory in the generated SDK ZIP package. 

If you ask about sources of the FreeMASTER desktop applications, then the answer is no. The sources are not publicly available.

Best regards,

Michal

在原帖中查看解决方案

0 项奖励
回复
1 回复
3,186 次查看
MichalH
NXP Apps Support
NXP Apps Support

Dear Stepan,

the source code of FreeMASTER serial and CAN communication driver is available in the MCUXpresso SDK. The source code is the same for all MCUs supported by the SDK, so just pick any of the supported devices or boards (e.g. FRDM-K64F) and add the FreeMASTER  middleware component. The sources will be located in middleware/freemaster directory in the generated SDK ZIP package. 

If you ask about sources of the FreeMASTER desktop applications, then the answer is no. The sources are not publicly available.

Best regards,

Michal

0 项奖励
回复