The FlexIO seem to be one of the big plusses of the i.MX RT1010.
Am I reading the schematic correctly that the FlexIO pins are not broken out to the Arduino Sheild pins?
Maybe there are more muxing features than I understand.
Hi James
FLEXIO is not specifically fanned out to Arduino interface.
The following flexio pins can be used in RT1010 connectors.
GPIO_AD_09
GPIO_AD_10
GPIO_AD_14
GPIO_08
GPIO_09
GPIO_10
Please pay attention to the signal, some pin route to the connector needs to add 0 resister.
Hi Lucas,
Can you specify what do you call RT1010 connectors?
I could not find how those pins you mention are connected ?
I thou can see some connections from FlexIO pins thru 0 ohm resistors to the arduino pins, but those might need a removal of a 0 ohm resistor, for instance, signal FLEXPWM1_PWMB0 seems to be available using pin 13 of J60 and at pin 12 of J56 thru R56, but what I suspect is that in order to use it, you need to disconnect SAI1_RX_BCLK from GPIO_01 and connect GPIO_01 to FLEXPWM1_PWMB0 using R793 .
Does this makes sense?
Please let us know,
Many thanks,