MC56F8037 SPI problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC56F8037 SPI problem

Jump to solution
2,365 Views
jithinrajnj
Contributor I

I Have been trying to communicate my MC56f8037 DSC to a LTC6803 battery stack monitor IC through SPI communication. DSC is intented to act as a SPI master. I tried processor expert bean SyncroMaster for SPI communication. But reading values from the slave gave me incorrect values. Later I used a different SPI function other than processor expert function .But now I'm getting some values when reading from ve but those are also incorrect. Now I suspect my spi writing function also wrong.

 

SPI is working in MODE3 with 500Khz clock rate. SPI functon for reading and writing is

 

#define SPIReadStatReg() (void)QSPI0_SCTRL;  // Clear Status reg.

#define SPIReadDataReg() (void)QSPI0_DRCV;  // Clear Data reg

#define SPIWaitReceiveDone()        while ((QSPI0_SCTRL&(0x01U<<3))) // Wait for full buf (SPRF)

#define SPIWaitTransferDone()       while (!(QSPI0_SCTRL&(0x01U<<0)))//Wait for buf empty  (SPTE)

 

 

void SPI_send_byte(unsigned char data)

{

  SPIWaitTransferDone();      // Wait for buf empty

  SPIReadStatReg();           // Read status register (possible SPRF, SPTEF) 

  SPIReadDataReg();           // Read receive data register. It clears flags

  QSPI0_DXMIT = data;              // Start transfer - send byte

  SPIWaitTransferDone();      // Wait for transfer complete

  SPIReadDataReg();

  SPIWaitReceiveDone();       // Wait for receive complete

}

 

unsigned char SPI_read_byte(void) 

{

   unsigned char value=0;      // function cannot directly return register value

   SPIReadStatReg();           // Read status register (possible SPRF, SPTEF) 

   SPIReadDataReg();           // Read receive data register. It clears flags                

  /QSPI0_DXMIT =0x00;   // Generate clocks for reading 1 byte of data!

   value = QSPI0_DRCV;

   SPIWaitReceiveDone();       // Wait for receive complete

   return(value);

}

please correct me if im wrong with these functions and also suggest a better and a reliable method to establish SPI communication with a DSC master and any other slaves.

Labels (1)
0 Kudos
Reply
1 Solution
2,172 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jithin,

As you know that the SPI uses synchronous protocol, it transmit data and receive data simultaneously, so you code is correct to read/write data by either checking the SPRF or SPTEF, not both.

I have browsed the SPI  timing of LTC6803, I do not know what is mode 3. It seems that the SPI of LTC6803 only supports the mode:CPHA = 1  CPOL = 1, in the mode, the /CSBI falling edge CAN NOT trigger the MISO signal valid,(the edge of SCKI make the MISO bit valid), the drawback of the mode is that the received data bit may disorder or lose synchronization, i do not know if it is your problem.

Hope it can help you

BR

XiangJun Rong

View solution in original post

0 Kudos
Reply
1 Reply
2,173 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jithin,

As you know that the SPI uses synchronous protocol, it transmit data and receive data simultaneously, so you code is correct to read/write data by either checking the SPRF or SPTEF, not both.

I have browsed the SPI  timing of LTC6803, I do not know what is mode 3. It seems that the SPI of LTC6803 only supports the mode:CPHA = 1  CPOL = 1, in the mode, the /CSBI falling edge CAN NOT trigger the MISO signal valid,(the edge of SCKI make the MISO bit valid), the drawback of the mode is that the received data bit may disorder or lose synchronization, i do not know if it is your problem.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply