MCF51JE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF51JE

767 次查看
Vick
Contributor I

I'm working in a project using MCF51JE256. Now i need send data through a ethernet port (RJ-45, socket conection),  is it possible do this using this MCU?

Thanks..

 

Eduardo

标签 (1)
2 回复数

662 次查看
chary
Contributor I

Hi,

You can do this with MCF51CN256 , I have implemented SPI to Ethernet bridge in my application using MCF51CN128.

Regards,

Chary

0 项奖励
回复

662 次查看
TomE
Specialist II

Anything is possible. You could add an external Ethernet controller to the Mini-FlexBus. You might be able to find a USB-connected Ethernet adaptor. But you can't get Ethernet on that chip without external hardware. Any "non-standard" solution would make the software a lot harder to get working.

The only MCF51 chip with Ethernet is the MCF51CN128. That has half the FLASH, less than half the RAM and a different mix of peripherals to the one you're using (no USB for instance).

You may need to step up to an MCF52 series chip.

Then you'll need a lot of extra software to get the network stack (e.g. FNET) unless you're already using something like MQX.

Tom