Coldfire v7.0 SE for MCF54455x License?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Coldfire v7.0 SE for MCF54455x License?

1,769件の閲覧回数
simath
Contributor I
I downloaded the CF v7.0 Special Edition (128k limited) from the MCF54455x product page a couple of months ago, and have only recently tried to use it again.  I can't compile - get an error message indicating that the license has expired.  I never attempted to get a license upon installing this product.  Now, if I go to the evaluation license page (License Activation System), there is no option for this product (CF only, "free" version).  So...  What do I need to do to get a license for this?  Note:  I mostly use the Linux development tool chain, but the Windows CF version is nice for some quick debugging, so I'd like to get this working again.  When the MCF54455x EVB first came out, there was a link on the product page to the V7.0 CF version (under Current Updates & Releases).  Now it appears the only way to get there is to go through the CW for CF page.  There is an updated version (12/14/2007) of the SE which can be downloaded.  Is this version really "free", forever, or is there a timeout?
 
 
ラベル(1)
0 件の賞賛
返信
1 返信

1,117件の閲覧回数
simath
Contributor I
OK, after installing the NEW (12-14-07) version of CW 7.0 for CF, it appears that the license.dat file is now "permanent", whereas it was set to expire on 12-31-07 on the previous version.  So, I guess the first version was a BETA or something that had an expiration tag?
0 件の賞賛
返信