Hi there, I'd be interested to know when a solution is found to this.
We use CodeWarrior MobileGT V9.2 for PowerPC and have a similar problem on 2 installations (we have 10 in total I think).
One one installation, when the uses wants to enter debug, we get the following error "Windows no disk, exception processing message........."
Press cancel 8 times and the download starts, then when the download finishes the error appears again so we press cancel to enter the debugger.
The other system with a problem behaves exactly the same, but from memory the error message is slightly different.
Cheers
I just got this message on CodeWarrior Coldfire v7.1. It was rather annoying, but this is how I "fixed" it in my case. I removed all CDs from my system. I closed out of all my projects and files in CodeWarrior so it was blank. I then pulled out the USB port that was attached to my 52259Demo board. I restarted the computer. I opened up CodeWarrior and opened my projects. (The next step may or may not be necessary). I tried to connect to the debugger which of course failed since it wasn't plugged in. I connected the USB port to the DEMO card. I then burned the flash and I didn't get the error.
Hopefully this helps somebody else.
-Hugh
Well this is wierd.
I got fed up and so closed CodeWarrior, put a music CD in the drive, loaded the project from a backup and it now runs.
Take the CD out and all is still ok.
So whatever it is does go away if 'any' CD is put in the drive.
It was "Lady Antebellum" .. not bad.
Hi Folks,
I am using IDE version 5.9.0 build 3024 developing for a MCF54450 board.
Out of the blue I am now getting this same error as you guys.
---------------------------
LHintAttachment: IDE.EXE - No Disk
---------------------------
There is no disk in the drive. Please insert a disk into drive D:.
---------------------------
Cancel Try Again Continue
---------------------------
All I was doing was changing the debugger settings for the project .. probably just a coincidence, but by crickey this is a sod of a problem!
Has a work around been determined?
Cheers
Was the "No Disk" issue resolved? If so, what is the workaround?
I'm also getting it, and it's really terrible. Here are my details:
LHintAttachment: IDE.EXE - No Disk
There is no disk in the drive. Please insert a disk into drive D:.
It doesn't happen when I load the project, it happens when I click the Debug button to start debugging. But it only happens the first time I start debuggging. (But see below for why this is still really horrible for my situation.)
I'm using CW for the Wii. Help -> About shows:
CodeWarrior IDE version 5.9.0
Build 3314
I've attached a copy of the Installed Plugins file.
Unfortunately, in my situation this error message is insanely irritating. I have to exit CodeWarrior every time I want to compile, since I am not using CodeWarrior for my compiles, and CodeWarrior loves to have a lock on the exxecutable file, even after you stop debugging.