T1024 booting issue : codewarrior Failed to correctly configure the JTAG chain(CCSProtocolPlugin)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1024 booting issue : codewarrior Failed to correctly configure the JTAG chain(CCSProtocolPlugin)

794 Views
Sayidathahaseen
Contributor II

Hi  team,

We have  designed customised board with reference to T1024rdb.
From codewarrior tool,we are able to flash image files to bare boards for the first time but not able boot(no logs from debug console).
Later  we are not able to flash them from code warrior.

We are getting following JTAG connection error.

Error: Connect Failed.
Failed to correctly configure the JTAG chain(CCSProtocolPlugin)
Error: Connect Failed.

log v output is attached for your reference.

 

Many thanks,

Syeda

0 Kudos
Reply
1 Reply

745 Views
yipingwang
NXP TechSupport
NXP TechSupport

It seems that there is no valid RCW on the target board.

Please refer to section "4.7.5.1.1 Hard Coded RCW Options" in T1024 Reference Manual to configure the your custom board as hard-coded RCW.

0 Kudos
Reply