CodeWarrior cw_dbg.flt.elf2flt error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior cw_dbg.flt.elf2flt error

1,844 Views
jarjarbin
Contributor I
Hi,

I'm a newbie, if anyone has an answer, I would appreciate. I have used the linux stationnery wizard to create a simple soft for coldfire device. When I try to compile the project, I get the following error:

link error /usr/local/m68k-elf/bin/ld.real : can not open /test/cw_dbg.flt.elf2flt no file or folder
link error   ld return 1 exit status

thx!

Labels (1)
0 Kudos
Reply
1 Reply

427 Views
Alban
Senior Contributor II
Hello,

You provide too little information.
Please read the post: [IMPORTANT] When Asking about CODEWARRIOR !!!

We need the targetted MCU to figure in the subject line.
Finally, the subject line is required to mean something.

Thank you,
Alban.


Message Edited by Alban on 2007-06-27 03:13 PM
0 Kudos
Reply