CodeWarrior cw_dbg.flt.elf2flt error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior cw_dbg.flt.elf2flt error

1,713件の閲覧回数
jarjarbin
Contributor I
Hi,

I'm a newbie, if anyone has an answer, I would appreciate. I have used the linux stationnery wizard to create a simple soft for coldfire device. When I try to compile the project, I get the following error:

link error /usr/local/m68k-elf/bin/ld.real : can not open /test/cw_dbg.flt.elf2flt no file or folder
link error   ld return 1 exit status

thx!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

296件の閲覧回数
Alban
Senior Contributor II
Hello,

You provide too little information.
Please read the post: [IMPORTANT] When Asking about CODEWARRIOR !!!

We need the targetted MCU to figure in the subject line.
Finally, the subject line is required to mean something.

Thank you,
Alban.


Message Edited by Alban on 2007-06-27 03:13 PM
0 件の賞賛
返信