CodeWarrior V6.4 for ColdFire; Flash Programmer can't calculate checksum.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior V6.4 for ColdFire; Flash Programmer can't calculate checksum.

1,858 次查看
Claude_Sylvain
Contributor I
Hello,
 
I use CodeWarrior V6.4 for Coldfire.
The target I use is a MCF52223 MCU.
CodeWarrior is running over Windows XP professionnal.
 
The problem happen when using the "Flash Programmer" tool, and can be describe as follow:
 
When using the Flash Programmer tool to calculate a checksum with the option "Compute Checksum Over..."->"Memory Range on Target" selected, and the "Address Range"->"Start: 0x" set to a value other than "00000000", the operation fail all the time.
When this value is set to "00000000", all is working correctly.
 
Is it possible that this tool can only calculate checksum starting from 0x00000000 !?
Or, is there something I am missing ?
 
 
Claude.
Electro-Technica inc.
 
 
标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

467 次查看
CrasyCat
Specialist III
Hello
 
I would recommend you to submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.

Attach the generated .zip file to the SR.
 
CrasyCat
0 项奖励
回复

467 次查看
Claude_Sylvain
Contributor I
Hello CrasyCat,
 
I just submited a service request for that issue.
 
Thank you.
Claude.
Electro-Technica inc.
 
0 项奖励
回复