CW 8.1 WireTAP errors connecting to Lite5200b

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 8.1 WireTAP errors connecting to Lite5200b

1,532 Views
rrorden
Contributor I
Our Lite5200b Rev H board lost its U-boot loader, so I installed CW 8.1 on Win2k and followed instructions to re-program flash with the original dBUG image using WireTAP. When I tried to do a blank check it fails and the CCS log shows these errors:
...
CCS: 03B8 : ccs_config_chain
CCS:  :  serverh = 0
CCS:  :  cc = 0
CCS:  :  device_list: (size = 1)
CCS:  :   device[0]:: core_type=36; device_descr=[ir_length:0;dr_bypass_length:0;bypass_instruction:0]
CCS:  : ccs_config_chain; ccs_error = 24
CCS:  :  Error message:
CC driver failure
CCS: 03B8 : ccs_delete_cc
CCS:  :  serverh = 0
CCS:  :  count = 0
CCS:  : ccs_delete_cc; ccs_error = 6
CCS:  :  Error message:
Invalid parameter
CCS: 03B8 : ccs_kill_server
CCS:  :  serverh = 0
CCS:  : ccs_kill_server; ccs_error = 0
Then I tried building the sample HelloWorld and debugging it on the board via WireTAP and it got the exact same error log. I confirmed the BIOS parallel port setting is ECP mode. When I disconnect WireTAP from the 5200 board I get the same error log. Also the same log when I power off the WireTAP. So I don't think it is a board-level or WireTAP h/w problem. Could something be preventing the parallel port from working? I looked at the Zeecube driver in the device settings and it says it is working properly. Any ideas?
 
 
 
Labels (1)
0 Kudos
Reply
1 Reply

541 Views
Voxan
Contributor III
Hi there,

I'm not sure the recent versions of CW support WireTAP any longer, USB-TAP and Ethernet TAP are the  current supported HTIs.

Could you please log this request to the support line at:

 http://www.freescale.com/webapp/sps/site/homepage.jsp?nodeId=054670&tid=t8dr#online_assisted

and click the link "Submit a service request online".


0 Kudos
Reply