Hello,
For MC68HC908AB32 microcontroller which CodeWarrior version is required? . what is the difference between CW IDE 6.3.2 and CW for MCU 11.1.?
Thanks and Regards
Pooja Katariya
HI,
MC68HC908AB32 is very old product. It is only supported on CW6.3 now:
CW6.3 is legacy product. It works on Windows XP/Vista 32-bit , but doesn't support win7/10/11 64bit.
CW for MCU 11.1 doesn't support HC08 device. It supports HCS08.
Hope this helps,
Jun Zhang
Hi
for this MC68HC908AB32 , which exe file should I download, In below link here is so many file is showing.
https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=5901331
I can't open this link. Please send me a screenshot. Thanks.
Hi Zhang Jennie.
If I am installing CodeWarrior for Microcontrollers (RS08HC(S)08-ColdFire V1) v6.3.exe for MC68HC908AB32CFU In my Machine which have XP window then this below error is coming.
Do you have any idea why this error is coming.
Thanks and Regards
Pooja Katariya
This is an another question. To saperate different subject, please create a new thread to ask with the problem screenshot.
Thanks,
Jun Zhang
I am not able to download the link which you have shared for CodeWarrior version.
Can you please share the details which version should I download in XP Pc for MC68HC908AB32CFU.
Thanks for your revert ,
Is there any product available which is compatible with this MC68HC908AB32 product. If it is available then we can replace this product.
Thanks and Regards
Pooja Katariya
Hi PoojaKat123,
There is no pin to pin device to MC68HC908AB32. I suggest LPC80x device as replacement.
LPC80x build toolchain is MCUXpresso IDE.
Hope this will help you,
Jun Zhang
Hi,
Thanks for your response, this product series is available for 64 pin or not?
Hi PoojaKat123
No. If 64pin is must, I suggest LPC845M301JBD64 or LPC844M201JBD64
https://www.nxp.com/part/LPC845M301JBD64#/
https://www.nxp.com/part/LPC844M201JBD64#/
LPC845 supports DAC and cap touch, LPC844 doesn't. Other features are the same.
Hope this helps,
Jun Zhang
Hi,
Thanks for your suggestion , Which microcontroller you have suggested these have all features of MC68HC908AB32CFU, like Keyboard Interrupt , SCI transmit and receive features.
Thanks and Regards
Pooja Katariya
The most similar part should be KE02. It also has 64k package.
Hope this helps,
Jun Zhang
Hi ,
Is there any microcontroller which is compatible with MC68HC908AB32CFU.
because these suggested microcontroller do not have all features and also do not have EEPROM , Monitor ROM.
Thanks and Regards
Pooja Katariya
Hi,
I there any microcontroller which have pin to pin connection these microcontroller not pin to pin.
Thanks and Regards
Pooja Katariya
NO, we don't have pin to pin replacement for this part.