MULTILINK UNIVERSAL Rev.B is not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MULTILINK UNIVERSAL Rev.B is not working

881件の閲覧回数
vigneshkumarp
Contributor III

Hi, I am using MULTILINK UNIVERSAL Rev.B. The programmer is working at some time not at most times.

When I used to program it works fine for some times but after that it stops working.

 

The same target board is working fine with another MULTILINK UNIVERSAL Rev.C.

 

What should I do now to rectify this problem?

 

173979_173979.jpgpastedImage_4.jpg

173978_173978.JPGCapture.JPG

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

673件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi VIGNESHKUMAR P

Could you tell us what CodeWarrior version, OS and MCU are you using? Also, Have you tried to installed P&Emicro drivers in your IDE?

Regards

Jorge Alcala

0 件の賞賛
返信

673件の閲覧回数
vigneshkumarp
Contributor III

Hi Jorge Antonio Alcala Vazquez,

Am using CW 10.6 under windows 7 and controller is KINETICS MKV10Z32VLC7(Using PORT-B in multilink). Yes I have Installed the latest P&E micro drivers.

And now the Universal Multilink is programming good for 5 to 10 times but afterwards it stops and shows the above error.

Regards,

Vigneshkumar P

0 件の賞賛
返信