MCF51QE128 with SD Card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF51QE128 with SD Card

932件の閲覧回数
daltonaota
Contributor I

Hello !

 

I wonder if someone has already developed something using MCF51QE128 accessing a SD Card!

 

I need to read the contents of the SD Card , which will be images, record a RAM Serial to display on a TFT display ! If someone can help me , I will be very grateful !

 

Thank you

ラベル(1)
タグ(3)
0 件の賞賛
返信
6 返答(返信)

842件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Dalton,

yes, I did. The project is on GitHub here: mcuoneclipse/Examples/CodeWarrior/DEMOQE/FreeRTOS_MCF51QE128 at master · ErichStyger/mcuoneclipse · ...

It is using FatFS as described here: https://mcuoneclipse.com/2012/07/30/fatfs-with-kinetis/

(concept applies to ColdFire V1 too).

The project includes FreeRTOS v9.0.0 plus the latest FatFS (I have not published the latest component version for it yet, so I have attached the current source base).

It uses the McuOnEclipse components (see https://mcuoneclipse.com/2014/10/21/mcuoneclipse-releases-on-sourceforge/ ).

I hope this helps,

Erich

0 件の賞賛
返信

842件の閲覧回数
daltonaota
Contributor I

Hi Erich,

Thank your for reply!!! I going to see your project...

But, I work with CodeWarrior, I believe that is not a problem!

Thank you again,

Dalton.

0 件の賞賛
返信

842件の閲覧回数
BlackNight
NXP Employee
NXP Employee
0 件の賞賛
返信

842件の閲覧回数
daltonaota
Contributor I

Erich...

I think the version I use is to be different from the project that gave me ...

I still use CodeWarrior 6.3 ...

0 件の賞賛
返信

842件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Yes, I'm on 10.6.4 (with update 6).

That's the latest version.

Erich

0 件の賞賛
返信

842件の閲覧回数
daltonaota
Contributor I

Ah, ok Erich!

Thank you!

0 件の賞賛
返信