Is there a common compiler that runs under eclipse for 9s12 and coldfire that runs on Win7?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a common compiler that runs under eclipse for 9s12 and coldfire that runs on Win7?

1,170 Views
nikhilthiruveng
Contributor I

Hi Guys,

I want to know whether there is a common compiler that runs under eclipse, maybe, for 9s12 and ColdFire, that runs on Win7.

Are there compilers other than Codewarrior for 9s12 and Coldfire processors????

Thanks in advance.

N


Labels (1)
0 Kudos
Reply
1 Reply

1,044 Views
dataScout
NXP Employee
NXP Employee

Hello,

ColdFire build tools are integrated in CodeWarrior for MCU 10.x (which is Eclipse based) - this runs on Win7

S12 build tools are not integrated in Eclipse based CW, but the Classic CW (5.1 in S12 case) works under Win7 (but need to be installed under an accessible path (other than Program Files (x86)), or to be run as Administrator)

Regards

0 Kudos
Reply