How do I disable the "Always Erase and Program flash without asking" option in the Hardware Connection Advanced Programming Options?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I disable the "Always Erase and Program flash without asking" option in the Hardware Connection Advanced Programming Options?

1,010件の閲覧回数
mjosborne
Contributor II

Hello,

 

this is a re-post of Re: How do I disable the "Always Erase and Program flash without asking" option in the Hardware Conn... There is a separate issue around software breakpoints that is being addressed by our FAE; however, we would like to figure this out as it adds a lot of time when debugging...

 

So, in a CodeWarrior10.6 project, when we download our image to external RAM for debugging CodeWarrior always attempts to write to flash. This takes a long time to time-out and fail; we cannot disable this option. Help!

32812_32812.pngAdvanced_Programming_Options.png

ラベル(1)
0 件の賞賛
返信
1 返信

792件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Matt,

Apologies for the delayed response, I have just received confirmation from P&E that there is no way to disable the "Always Erase and Program flash without asking" option.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信