How and where to program and compile  an eMIOS and dump it to MPC5676R?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How and where to program and compile  an eMIOS and dump it to MPC5676R?

883 次查看
snehakalkhair
Contributor III

How and where to program and compile  an eMIOS and dump it to MPC5676R?

标签 (1)
标记 (1)
1 回复

769 次查看
martin_kovar
NXP Employee
NXP Employee

Hi,

for compile eMIOS code you can use for example:

CodeWarrior Dev Tools for MPC55xx/MPC56xx|NXP

CodeWarrior for Microcontrollers-Eclipse IDE|NXP

or

MULTI Integrated Development Environment

For flash the code could be used debug probes or standalone flashers.

With CodeWarrior could be used these debug probes:

Universal Multilink Development Interface|NXP

Universal Multilink FX High-Speed Development Inter|NXP

With MULTI IDE could be used

Multi-core JTAG, EJTAG, COP, BDM hardware assisted debugger, embeddeddebugging, on-chip debugging - ...

Also Lauterbach is possible to use as a flasher and debugger

TRACE32® Qorivva MPC5xxx and SPC5xxx Debugger

And as a standalone flasher I can recommend you Cyclone MAX

Cyclone MAX|NXP

Regards,

Martin