Hello, I am new on Freescale. I am surprise Codewarrior will be installed only in virtual machine Windows XP, not in a usual Windows 64 bit like Win7. Is this real?
Hi Henry,
Could you tell us which MCU are you using? If you are not using a legacy device there should be a new CodeWarrior version that supports Win 7.
Thanks in advance!
Best Regards,
Carlos Mendoza
Technical Support Engineer
I am using this
MC9S08SE8VWLE
Thank you nd best regards
Henry
Il 23/04/2018 22:19, Carlos_Mendoza ha scritto:
>
NXP Community
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
>
Re: Hello, I am new on Freescale. I am surprise Codewarrior will
be installed only in virtual machine Windows XP, not in a usual
Windows 64 bit like Win7. Is this real?
reply from Carlos_Mendoza
<https://community.nxp.com/people/Carlos_Mendoza?et=watches.email.thread>
in /CodeWarrior for MCU/ - View the full discussion
<https://community.nxp.com/message/1008077?commentID=1008077&et=watches.email.thread#comment-1008077>
>
Hi Henry,
For the MC9S08SE8 devices you can use CodeWarrior for MCUs (Eclipse IDE), which comes with host operating system support for Win XP, 7, 8, 8.1 and 10:
CodeWarrior for Microcontrollers-Eclipse IDE|NXP
Hope it helps!
Best Regards,
Carlos Mendoza
Technical Support Engineer
Ok I see now on my Win7.
Other question, I have Multilink Universal , is there a simle software
like programmer for hex files?
thanks
Henry
Il 24/04/2018 16:15, Carlos_Mendoza ha scritto:
>
NXP Community
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
>
Re: Hello, I am new on Freescale. I am surprise Codewarrior will
be installed only in virtual machine Windows XP, not in a usual
Windows 64 bit like Win7. Is this real?
reply from Carlos_Mendoza
<https://community.nxp.com/people/Carlos_Mendoza?et=watches.email.thread>
in /CodeWarrior for MCU/ - View the full discussion
<https://community.nxp.com/message/1008377?commentID=1008377&et=watches.email.thread#comment-1008377>
>