CW 4.7 for HCS12 with Vista

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 4.7 for HCS12 with Vista

2,409件の閲覧回数
ernestsnaith
Contributor I
I am having difficulties installing CW 4.7 on the only laptop I have available to me which runs Vista. I know there were issues with 4.6 and experienced them myself but is 4.7 supposed to be compatable? I currently get the failed to install INF file towards the end of the installation. I am desperate to get CW on this machine as i have a demo shortly. Is there a solution?
 
Cheers, Erny
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

626件の閲覧回数
ernestsnaith
Contributor I
No firewall at present, that annoyed me within minutes of buying laptop
0 件の賞賛
返信

626件の閲覧回数
J2MEJediMaster
Specialist I
From the info box on the CW for HCS12X 4.7 download page:

LIMITATIONS:

WINDOWS VISTA SPECIFIC LIMITATIONS:

The following limitations are applicable only if you are installing the product on Windows Vista:

1. During installation, security messages may pop up concerning drivers being installed. It is highly recommended to click on the option "continue anyway..", so the driver can be installed.

2. When opening the Codewarrior components (IDE, Debugger etc.) Firewall warnings may appear with the option to block or unblock the application. It is advisable to click on the unblock option to continue.

3. For more VISTA specific limitations after the installation, please refer to:
"{INSTALLATION DIRECTORY}\Release_Notes\HC12\Notes_CW_HC12_Vista.txt"

---Tom