Hi,
I have a LPC55S16-EVK, and my main goal is to connect 2 different machines to the EVK using USB ports.
1 machine connected to the USB Full-Speed port and 1 machine connected to the USB Hi-Speed port.
I need that both machines will detect the EVK as a USB device.
Currently, I'm able to detect the EVK as a USB device from my linux machine (connected to Full Speed USB port), using dev_composite_cdc_msc_bm exmaple.
Now, I would like to detect the Hi-Speed port as a USB device as well.
I'm looking for an example that uses both ports as USB devices.
Thanks
Solved! Go to Solution.
Hello,
There is a dual USB device project under the below thread:
https://community.nxp.com/t5/LPC-Microcontrollers/Use-LPC55S16-to-configure-two-USB-HID-generic-devi... (See attachment).
BR
Alice
Hello,
There is a dual USB device project under the below thread:
https://community.nxp.com/t5/LPC-Microcontrollers/Use-LPC55S16-to-configure-two-USB-HID-generic-devi... (See attachment).
BR
Alice
Thanks