cw 10.5 cyclone for ARM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cw 10.5 cyclone for ARM

2,046 Views
NicolaPonte
Contributor I


Dear Sirs,

 

I'm trying to use Cyclone for ARM as a debugger with CodeWarrior 10.5 and a K60 microcontroller.

I select it in debug options but it's seen as a Cyclone MAX. Then, I start debug but at the moment of downloading firmware into K60 memory, the "P&E Connection Assistant" window tells me that there is no device available.

Any suggestion? I'll contact PE Micro too.

8912_8912.pngimm1.png

8913_8913.pngimm2.png

 

 

Thanks

Labels (1)
Tags (5)
0 Kudos
Reply
2 Replies

1,924 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

seems the driver problem, please uninstall cyclone max driver from windows device manager when connecting

then reinstall it.

0 Kudos
Reply

1,924 Views
johnny_pe
Contributor III

Hi Nicola and Jennie,

Please note that the Cyclone for ARM stand alone programmer is currently NOT supported by Codewarrior. It will be supported by Codewarrior v10.6 Update 2.

Regards,

Johnny

P&E Microcomputer Systems

0 Kudos
Reply