Hi,everybody, I use MCS8157 at the moment, But some problems appear at the use of CodeWarrior TAP, The CodeWarrior TAP can't connects USB to the target boards debugger port, When the connection runs at 82%, a error is happend, that is ccs: core not supported or failed to reset the target. We have test the signals of poreset, hreset and hreset_in, when the poreset is deasserted, the device keep hreset low until after 1.975 seconds, that is it meets the requirement of 1.98 seconds in the MSC8157RM. We use the version 10.0. Please see the file attached. Thank you !
The MSC8157 is not support in CW10.0, and CWTAP(different from USBTAP) is not supported in CW10.0, please use CW10.5 for your case.
Please contact Freescale support if you do not have CW10.5, and let me know your SR number.