Hi all. I have a problem when I try to read some devices and ColdFire

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi all. I have a problem when I try to read some devices and ColdFire

385 Views
carmenhernandez
Contributor I

I'm using: CodeWarrior for ColdFire V7.2, MCF5235CVM150 processor, MULTILINK UNIVERSAL FX PEMICRO programmer and S29AL032D70 memories. I can't read S29AL032D70 series in CodeWarrior, only   S29AL016..., don't even recognize the ColdFire.  There's a way to add the algorithms? or How can I solved?  A hope your answer soon. Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

301 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Carmen

The S29AL008J55BFIR2 is not in the list of Flash_Programmer devices that supported:

Freescale\CodeWarrior for ColdFire V7.x

\ColdFire_Support\Initialization_Files

Please create it following 6.3 in AN3389:

http://cache.nxp.com/files/soft_dev_tools/doc/app_note/AN3389.pdf

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply