Codewarrior 10.1 with win7 64bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior 10.1 with win7 64bit

Jump to solution
2,412 Views
terra
Contributor I

Just down load and install CW 10.1 on Win7X64bit machine. I use the example project for HCS08 then import the projet then press re build all at it shows me error on main_asm on line 0

 

What could be the probelm?

Labels (1)
0 Kudos
Reply
1 Solution
1,155 Views
CrasyCat
Specialist III

Hello

 

It looks like the problem is related to the installation path.

Can you please Try to uninstall CodeWarrior and re-install it in a path without any space in the fullpath.

        For instance c:\Freescale

 

Is it working better?

 

If this is the case,  I would recommend you to submit a service request for that.

Spaces should be accepted in path names.

Click here to submit a service request.

CrasyCat

View solution in original post

0 Kudos
Reply
8 Replies
1,155 Views
CrasyCat
Specialist III

Hello

 

Which sample project are you using?

 

What is the message you are getting (Whole message please)?

 

CrasyCat

0 Kudos
Reply
1,155 Views
bla5029
Contributor I

Make sure win windows 7 you are running Codewarrior as administrator.

 

I have been working with the webserver demo I am also getting that error.  I notice that it will not give me normal errors for syntax mistakes.  This is the only error i have recieved.  Is there something configured wrong in my project?

0 Kudos
Reply
1,155 Views
terra
Contributor I

I try most of the example and giving me the same error

here is soem screen shots

0 Kudos
Reply
1,155 Views
CrasyCat
Specialist III

Hello

 

  1- Can you please copy content of the Console window and send it over?

      Console will contain more details than Problem view.

 

  2- If you are programming in assembler, directives and instructions cannot start on column 1.

      Please insert at least 1 space or TAB in front of the XDEF and include instruction.

 

CrasyCat

0 Kudos
Reply
1,155 Views
terra
Contributor I

1. Here is the attachement

2. Thanks for the info

0 Kudos
Reply
1,156 Views
CrasyCat
Specialist III

Hello

 

It looks like the problem is related to the installation path.

Can you please Try to uninstall CodeWarrior and re-install it in a path without any space in the fullpath.

        For instance c:\Freescale

 

Is it working better?

 

If this is the case,  I would recommend you to submit a service request for that.

Spaces should be accepted in path names.

Click here to submit a service request.

CrasyCat

0 Kudos
Reply
1,155 Views
terra
Contributor I

Thanks mate, it is working fine with C:\FreeScale

0 Kudos
Reply
1,155 Views
bla5029
Contributor I

had that problem with 10.0, and changing the direction path for the project seems to work as well.  The MQX was looking in program files, not program files x86, just throw the x86 in on the path and it picks up and runs with it.

0 Kudos
Reply