CodeWarrior profiler for 56F8366 (56800E core)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior profiler for 56F8366 (56800E core)

2,324 次查看
admin
Specialist II

Hi,

I'm trying to set up profiler for 56F8366 MCU. I follow the "CodeWarrior™ Development Studio IDE 5.5 User’s Guide Profiler Supplement" and CW help. I also tried to find something on forums - no result. If option "generate code for profiling" is not selected in CW settings, I (sometimes) have the file in my output dir, but it's empty. When I select that option, debugger stops somewhere before entry point (code is not executed). Any hints?

TIA Bartek

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,052 次查看
trytohelp
NXP Employee
NXP Employee
Hi,
 
You meet problem to use the profiler feature.
Can I suggest you to have a look to the IDE_5.5_UG_Profiler.pdf manual in the \Help\PDF folder ?
 
There're an example on the installation.
\(CodeWarrior_Examples)\SimpleProfiler
 
Hope this will help you.
 
Pascal
0 项奖励
回复

1,052 次查看
CrasyCat
Specialist III
This discussion was moved to a better location.
0 项奖励
回复