Temperature compensation on MC9S08QB4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Temperature compensation on MC9S08QB4

ソリューションへジャンプ
583件の閲覧回数
benthie
Contributor II

Hi erveryone,

 

I´m about to implement a temperature compensation on a MC9S08QB4. I already read the application note AN3031 in order to get some information about how to get a higher accuracy and the calibration procedures. So far so good.

 

I think I also understood, that for my application the knowledge of an exact temperature is not important. The ADC value of the sensor is enough to compensate the error due to temperature changes !?

 

What I definitely do not understand is whether I have to bring the sensor value in relation to the current bandgap value or not. In other words: do I have to determine current V_DD by using the bandgap voltage in order to get a accurate sensor reading V_TEMP or is it nonsense in this case?

 

Regards,

Ben

ラベル(1)
0 件の賞賛
返信
1 解決策
457件の閲覧回数
pavel_sadek
NXP Employee
NXP Employee

Hi Ben

For different supply voltages you will get different ADC readouts - see the figure 1 of the AN3031, you need to know the supply voltage as Vtemp25 is stated for 3V supply in the datasheet.

So you need to know the correct supply voltage - the band gap voltage reference will help you to figure out (measure) what is the correct supply voltage (you will get ADC representation of 1.17V) and this way, you can recalculate ADC readout correctly to junction temperature of the chip.

there is also code for the AN attached in Freescale pages, so you can adapt it more easily to your MCU/ board.

Pavel

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
458件の閲覧回数
pavel_sadek
NXP Employee
NXP Employee

Hi Ben

For different supply voltages you will get different ADC readouts - see the figure 1 of the AN3031, you need to know the supply voltage as Vtemp25 is stated for 3V supply in the datasheet.

So you need to know the correct supply voltage - the band gap voltage reference will help you to figure out (measure) what is the correct supply voltage (you will get ADC representation of 1.17V) and this way, you can recalculate ADC readout correctly to junction temperature of the chip.

there is also code for the AN attached in Freescale pages, so you can adapt it more easily to your MCU/ board.

Pavel

0 件の賞賛
返信