Hi,
I need to program a MC9S08SH8 microcontroller with Codewarrior 6.3.
In the past I used PEmicro and I set 32MHz in the DCO Output frequency (see picture attached).
At the moment I don't have the possibility to use PEmicro and I would like to maintain this setting also on Codewarrior.
Is there this possibility?
Thank you in advance.
Hi Vincente,
regarding my first question: exactly, I can't set the clock properly using the OSBDM in the demo board. I don't know why.
Regarding USBDM: actually I've found this open source project
https://sourceforge.net/projects/usbdm
and I bought an USBDM interface on ebay.
I would like to know if it's recognize as a reliable instruments by NXP.
Thank you and Best Regards,
Mattia
Hi Mattia
I do not use that tool so I can not say this is good or not.
regarding to your problem with the OSBDM maybe you need to update it
You can update with the driver from PEMICRO
I hope this will help you.
Hi Vincente,
thank you for your answer.
Actually I'm using this evaluation board to program the microcontroller:
I've already tried to modify the parameter in debug configuration but it has anyway an higher clock. I can understand it because the answer in the UART port is faster than 9600kbps (as setted). It seems almost 5% higher.
In parallel I've tried to use the USBDM interface with its software. With its clock trimming setup it works!
So, what I would like to know is:
-why the evaluation board can't set the correct clock frequency?
-Is in your opinion the USBDM interface reliable for programming? Also for production? I'm asking this because it seems that it's an open source hardware and software.
Thank you for your attention and best regards,
Mattia
Hi
I am not sure that I got properly your first question, but you can not set properly the clock using the OSBDM that is included on the demo board?
regarding your second question, the USBDM (the universal multilink?), can work for production, but if you have a high volume I recommend the cyclone
Regards
Hi
you can use Processor expert or device initialization, but this is creating a code.
Also there is a tool that you can set the TRIM value, maybe this can help you, you can set the internal clock with a value between 31.250 to 39062.5 Hz please check the image attached.
Debug configuration/edit/ advance programming options / use custom trim...
Hi
I am not sure if the tool that you was using is the flasher from PE?
so now you want something similar with code warrior 11?
Please let me know your comments
Regards
Vicente