Neil -
The Processor Expert bean is correct. The flash locations for the trim are $FFAE and $FFAF. $FFBE and $FFBF are wrong. (In fact, $FFBF is the NVOPT register.)
The issue is with the SofTec programmer. There is a fix so that it puts the trim value in the right location. The fix is in the attached zip file. Upzip it and place the "SofTec_BDC08.DLL" in the following CodeWarrior directory (replacing the existing file):
C:\Program Files\Metrowerks\CW08 V3.1\prog (assumes that you installed to the default locations)
BTW - This is fixed in CodeWarrior08 5.x
- Rocky
Message Edited by RockyRoad on 2006-08-29 03:31 PM