| | |
| Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for S32 Platform v3.2 | 
|
| | |
Austin, Texas, USA Sep 30, 2019 | The Automotive Microcontrollers and Processors' Embedded Tools Team at NXP Semiconductors is pleased to announce the release of the S32 Design Studio for S32 Platform v3.2. Here are some of its major new features: - Multiple builds of the GNU tools can be installed.
- The SDK integration is provided with additional software packages. The SDK packages can be installed and updated with the S32DS Extensions and Updates tool.
- The GHS toolchain support is provided by the project wizard (available for particular devices).
- The CMSIS-DAP debugging is supported by particular devices.
- The UART communication speed of S32 Flash Tool is improved.
- The latest versions of P&E debugger plug-in and drivers are provided.
- S32 Debugger provides OS Awareness support for FreeRTOS and OSEK.
- S32 Debugger provides preliminary support for secure debugging with the Password and Challenge/Response authentication methods.
- New type of Launch Groups is defined for S32 Debugger, which allows you to create S32 Debugger specific configurations and use the new "Wait for stop on breakpoint" post launch action.
- The SDK migration support is provided to upgrade an SDK version attached to the project.
- The S32DS Extensions and Updates tool notifies about dependencies and incompatible packages.
- The progress bar is displayed for the S32 Debugger flash programmer.
S32 Design Studio Versions | S32DS IDE for S32 Platform | S32DS IDE for Arm | S32DS IDE for Power Architecture | S32DS IDE for Vision | Devices Supported | S32V23x | S32K1xx | MPC56xx | S32V234 | S32S247TV | KEA | MPC57xx | | S32 Platform Devices | MAC57D54H | S32R2xx/S32R3xx | | Integrated NXP Tools | S32 Flash Tool | FreeMASTER | FreeMASTER | DDR stress tool | DDR stress tool | | | | Integrated Configuration Tools | S32 Configuration Tools | Processor Expert Configuration Tool | Processor Expert Configuration Tool | DDR configuration tool | Pins Wizard | Pins Wizard | Pins Wizard | | Clocks configuration | Peripheral/Drivers configuration | Peripheral/Drivers configuration | Peripheral/Drivers configuration | | DCD/IVT configuration | | | | DDR configuration tool | | | | Integrated NXP Software | S32 SDK | S32K1 SDK | S32 SDK | Vision SDK | FreeRTOS | FreeRTOS | FreeRTOS | Linux BSP | AMMCLib for S32V23x | AMMCLib for KEA and S32K | AMMCLib for MPC56xx and MPC57xx MCUs | | Vision SDK | KEA SDK | Radar SDK | | Linux BSP | MQX OS/MQX Drivers for MAC57D54H | | | Compilers: | NXP GCC 6.3.1* | NXP GCC 6.3.1* | NXP GCC 4.9* | NXP GCC 6.3.1* | GreenHills | GreenHills | GreenHills | | IAR | IAR | Diab | | | GCC 4.9* | | | DEBUGGERS Built-in GDB interface: | S32 Debugger/S32 Debug Probe | P&E Multilink/Cyclone/OpenSDA | P&E Multilink/Cyclone/OpenSDA | S32 Debugger/S32 Debug Probe | P&E Multilink/Cyclone/OpenSDA | Segger J-Link | | P&E Multilink/Cyclone/OpenSDA | DEBUGGERS supported: | Lauterbach | Lauterbach | Lauterbach | Lauterbach | | iSystem | iSystem | | | IAR | PLS | | Host Operating Systems: | Microsoft Windows 7/8/10 64-bit OS (with 32-bit binaries) – Ubuntu 14.04, 16.04 (64 bit) – Debian 8 (64 bit) – CentOS 7 (64 bit) | Microsoft Windows 7/8/10 32/64-bit OS (with 32-bit binaries) – Ubuntu 14.04, 16.04 (64 bit) – Debian 8 (64 bit) – CentOS 7 (64 bit) | Microsoft Windows 7/8/10 32/64-bit OS (with 32-bit binaries) – Ubuntu 14.04, 16.04 (64 bit) – Debian 8 (64 bit) – CentOS 7 (64 bit) | Microsoft Windows 7/8/10 32/64-bit OS (with 32-bit binaries) – Ubuntu 14.04, 16.04 (64 bit) – Debian 8 (64 bit) – CentOS 7 (64 bit) | Vision specific tools : | NXP APU Compiler | | | NXP APU Compiler | ISP assembler | | | ISP assembler | ISP and APEX graph tools | | | ISP and APEX graph tools | Radar specific tools : | | | SPT assembler | | | | SPT Explorer/ SPT graph tool | |
Complete S32 Design Studio for S32 Platform v3.2 release notes are available here. InstallationTo download the installer please visit the S32 Design Studio product page download section or click the direct here. 
The installer requires the Activation ID to be entered. You should receive a notification email including the Activation ID after the download of the installation package starts. The installer installs just the base tools/package. In order to start development it is necessary to install at least one Development package. Currently the only application packages available are S32S2xxTV and S32V2xx. The application packages are managed by S32DS Extensions and Updates. 
Technical SupportS32 Design Studio issues are tracked through the S32DS Public NXP Community space. | |
1 person found this helpful
how to get the "Visual Graph Tools" installed in the "New" wizard in v3.2? The pic below was from S32DS 3.1.
Thanks,
jd