S32 Design Studio for S32 Platform 3.2 (Windows/Linux) released!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for S32 Platform 3.2 (Windows/Linux) released!

S32 Design Studio for S32 Platform 3.2 (Windows/Linux) released!

 

 

 

nxp.png 

Product Release Announcement

Automotive Microcontrollers and Processors

S32 Design Studio for S32 Platform v3.2

pastedImage_1.png

 

 

 

 

Austin, Texas, USA

Sep 30, 2019

 

 The Automotive Microcontrollers and Processors' Embedded Tools Team at NXP Semiconductors is pleased to announce the release of the S32 Design Studio for S32 Platform v3.2.  Here are some of its major new features:

  • Multiple builds of the GNU tools can be installed.
  • The SDK integration is provided with additional software packages. The SDK packages can be installed and updated with the S32DS Extensions and Updates tool.
  • The GHS toolchain support is provided by the project wizard (available for particular devices).
  • The CMSIS-DAP debugging is supported by particular devices.
  • The UART communication speed of S32 Flash Tool is improved.
  • The latest versions of P&E debugger plug-in and drivers are provided.
  • S32 Debugger provides OS Awareness support for FreeRTOS and OSEK.
  • S32 Debugger provides preliminary support for secure debugging with the Password and Challenge/Response authentication methods.
  • New type of Launch Groups is defined for S32 Debugger, which allows you to create S32 Debugger specific configurations and use the new "Wait for stop on breakpoint" post launch action.
  • The SDK migration support is provided to upgrade an SDK version attached to the project.
  • The S32DS Extensions and Updates tool notifies about dependencies and incompatible packages.
  • The progress bar is displayed for the S32 Debugger flash programmer.

S32 Design Studio Versions

 

S32DS IDE for S32 Platform

S32DS IDE for Arm®

S32DS IDE for Power Architecture®

S32DS IDE for Vision

Devices Supported

S32V23x

S32K1xx

MPC56xx

S32V234

S32S247TV

KEA

MPC57xx

 

S32 Platform Devices

MAC57D54H

S32R2xx/S32R3xx

 

Integrated NXP Tools

S32 Flash Tool

FreeMASTER

FreeMASTER

DDR stress tool

DDR stress tool

 

 

Integrated Configuration Tools

S32 Configuration Tools

Processor Expert Configuration Tool

Processor Expert Configuration Tool

 DDR configuration tool

Pins Wizard

Pins Wizard

Pins Wizard

Clocks configuration

Peripheral/Drivers configuration

 

Peripheral/Drivers configuration

 

Peripheral/Drivers configuration

 

DCD/IVT configuration

 

 

 

DDR configuration tool

 

 

 

Integrated NXP Software

S32 SDK

S32K1 SDK

S32 SDK

Vision SDK

FreeRTOS

FreeRTOS

FreeRTOS

Linux BSP

AMMCLib for S32V23x

AMMCLib for KEA and
S32K

AMMCLib for MPC56xx
and MPC57xx MCUs

 

Vision SDK

KEA SDK

Radar SDK

Linux BSP

MQX OS/MQX Drivers for MAC57D54H

 

 

Compilers:

NXP GCC 6.3.1*

NXP GCC 6.3.1*

NXP GCC 4.9*

NXP GCC 6.3.1*

GreenHills

GreenHills

GreenHills

 

IAR

IAR

Diab

 

 

GCC 4.9*

 

 

DEBUGGERS
Built-in GDB
interface
:

S32 Debugger/S32 Debug Probe

P&E Multilink/Cyclone/OpenSDA

P&E Multilink/Cyclone/OpenSDA

S32 Debugger/S32 Debug Probe

P&E Multilink/Cyclone/OpenSDA

Segger J-Link

 

P&E Multilink/Cyclone/OpenSDA

DEBUGGERS supported:

Lauterbach

Lauterbach

Lauterbach

Lauterbach

 

iSystem

iSystem

 

IAR

PLS

 

Host Operating Systems:

Microsoft Windows® 7/8/10 64-bit OS (with 32-bit binaries) 

– Ubuntu 14.04, 16.04 (64 bit)

– Debian 8 (64 bit)

– CentOS 7 (64 bit)

Microsoft Windows® 7/8/10 32/64-bit OS (with 32-bit binaries) 

– Ubuntu 14.04, 16.04 (64 bit)

– Debian 8 (64 bit)

– CentOS 7 (64 bit)

Microsoft Windows® 7/8/10 32/64-bit OS (with 32-bit binaries) 

– Ubuntu 14.04, 16.04 (64 bit)

– Debian 8 (64 bit)

– CentOS 7 (64 bit)

Microsoft Windows® 7/8/10 32/64-bit OS (with 32-bit binaries) 

– Ubuntu 14.04, 16.04 (64 bit)

– Debian 8 (64 bit)

– CentOS 7 (64 bit)

Vision specific tools :

NXP APU Compiler

 

 

NXP APU Compiler

ISP assembler

 

 

ISP assembler

ISP and APEX graph tools

 

 

ISP and APEX graph tools

Radar specific tools :

 

 

SPT assembler

 

 

 

SPT Explorer/ SPT graph tool

 

Complete S32 Design Studio for S32 Platform v3.2 release notes are available here.

 

Installation

To download the installer please visit the S32 Design Studio product page download section or click the direct here.

 

pastedImage_56.png

 

The installer requires the Activation ID to be entered. You should receive a notification email including the Activation ID after the download of the installation package starts.

The installer installs just the base tools/package. In order to start development it is necessary to install at least one Development package. Currently the only application packages available are S32S2xxTV and S32V2xx. The application packages are managed by S32DS Extensions and Updates.

pastedImage_54.png

Technical Support

S32 Design Studio issues are tracked through the S32DS Public NXP Community space.

https://community.nxp.com/community/s32/s32ds

 

添付
コメント

how to get the "Visual Graph Tools" installed in the "New" wizard in v3.2? The pic below was from S32DS 3.1.

pastedImage_1.png

Thanks,

jd

Hello Jim,

The Visual Graph Tools comes as part of Vision Extension Package for S32V2xx v.1.0.0, however, this package is NOT SUPPORTED for S32 Design Studio v3.2. Please continue to use S32 Design Studio v3.1 until we release an updated version of the Vision Extension Package.

Best Regards,

Mike

評価なし
バージョン履歴
最終更新日:
‎09-30-2019 02:48 PM
更新者: