Hi everybody
I am redesigning custom circuit board using I.MX8 mini.
in the schematic of the IMX8mini EVK board using Audio IC WM8524 (Line out levels only for audio). but now I want to use MIC input and Headphone out, so which IC audio codecs can I use?
Can you suggest me?
Thank you
Solved! Go to Solution.
hi Rita Wang
Thanks for your help
I'm trying to use WM8960, but which DACLRC / BCLK sync signal can be connected to? SAI_TXFS / SAI_TXC or SAI_RXFS / SAI_RXC.
Sorry to bother, but please help
Many thanks
Hi,
Many IC you can use, such as WM8960, WM8962, SGTL5000.
Hope this can do help for you.
Have a great day,
Rita
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
hi Rita Wang
Thanks for your help
I'm trying to use WM8960, but which DACLRC / BCLK sync signal can be connected to? SAI_TXFS / SAI_TXC or SAI_RXFS / SAI_RXC.
Sorry to bother, but please help
Many thanks
You can refer to this https://community.nxp.com/docs/DOC-106295
thank you so much