Audio Codec IC for IMX8 mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Audio Codec IC for IMX8 mini

Jump to solution
3,930 Views
haryanl
Contributor IV

Hi everybody
I am redesigning custom circuit board using I.MX8 mini.
in the schematic of the IMX8mini EVK board using Audio IC WM8524 (Line out levels only for audio). but now I want to use MIC input and Headphone out, so which IC audio codecs can I use?
Can you suggest me?

Thank you

Tags (2)
0 Kudos
1 Solution
2,968 Views
haryanl
Contributor IV

hi Rita Wang
Thanks for your help
I'm trying to use WM8960, but which DACLRC / BCLK sync signal can be connected to? SAI_TXFS / SAI_TXC or SAI_RXFS / SAI_RXC.
Sorry to bother, but please help
Many thanks

pastedImage_1.png

View solution in original post

0 Kudos
4 Replies
2,968 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Many IC you can use, such as WM8960, WM8962, SGTL5000.

Hope this can do help for you.

Have a great day,
Rita

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
2,969 Views
haryanl
Contributor IV

hi Rita Wang
Thanks for your help
I'm trying to use WM8960, but which DACLRC / BCLK sync signal can be connected to? SAI_TXFS / SAI_TXC or SAI_RXFS / SAI_RXC.
Sorry to bother, but please help
Many thanks

pastedImage_1.png

0 Kudos
2,968 Views
Rita_Wang
NXP TechSupport
NXP TechSupport
0 Kudos
2,968 Views
haryanl
Contributor IV

thank you so much

0 Kudos