iMX6 SoloX MQX Kernel & Uboot Patches From AN5127

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 SoloX MQX Kernel & Uboot Patches From AN5127

Jump to solution
1,365 Views
jeremym
Contributor IV

I cannot locate the two patches mentioned in AN5127:

0001-Kernel-M4-Reserve-16M-DDR-memory-for-M4-core-use.patch

0001-U-Boot-M4-Reserve-16M-DDR-memory-for-M4-core-use.patch

Does anyone know where to locate these?

thanks,

jeremy

Labels (1)
Tags (3)
1 Solution
991 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jeremy McClintock,

These patches are no longer available on the git mentioned on the AN, but please find them attached.

Regards,

View solution in original post

5 Replies
991 Views
jeremym
Contributor IV

Hi Victor - any update on the location of the patches?  Thanks, Jeremy

0 Kudos
Reply
992 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jeremy McClintock,

These patches are no longer available on the git mentioned on the AN, but please find them attached.

Regards,

991 Views
jeremym
Contributor IV

Thank you very much, it's appreciated.

991 Views
b36401
NXP Employee
NXP Employee

You can get them with git as mentioned in the Application Note.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
991 Views
jeremym
Contributor IV

Hi Victor - the application note doesn't describe where to fetch the patch from.  It simply states to navigate to a particular folder and then attempt to apply the patch.  The patch was not part of the distribution when I fetched/cloned.  If I attempt to follow the application note as described, I get:

/usr/lib/git-core/git-am: 209: /usr/lib/git-core/git-am: cannot open 0001-Kernel-M4-Reserve-16M-DDR-memory-for-M4-core-use.patch: No such file