I cannot locate the two patches mentioned in AN5127:
0001-Kernel-M4-Reserve-16M-DDR-memory-for-M4-core-use.patch
0001-U-Boot-M4-Reserve-16M-DDR-memory-for-M4-core-use.patch
Does anyone know where to locate these?
thanks,
jeremy
解決済! 解決策の投稿を見る。
Hello Jeremy McClintock,
These patches are no longer available on the git mentioned on the AN, but please find them attached.
Regards,
Hi Victor - any update on the location of the patches? Thanks, Jeremy
Thank you very much, it's appreciated.
You can get them with git as mentioned in the Application Note.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Victor - the application note doesn't describe where to fetch the patch from. It simply states to navigate to a particular folder and then attempt to apply the patch. The patch was not part of the distribution when I fetched/cloned. If I attempt to follow the application note as described, I get:
/usr/lib/git-core/git-am: 209: /usr/lib/git-core/git-am: cannot open 0001-Kernel-M4-Reserve-16M-DDR-memory-for-M4-core-use.patch: No such file