Hello Jeremy McClintock,
These patches are no longer available on the git mentioned on the AN, but please find them attached.
Regards,
You can get them with git as mentioned in the Application Note.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Victor - the application note doesn't describe where to fetch the patch from. It simply states to navigate to a particular folder and then attempt to apply the patch. The patch was not part of the distribution when I fetched/cloned. If I attempt to follow the application note as described, I get:
/usr/lib/git-core/git-am: 209: /usr/lib/git-core/git-am: cannot open 0001-Kernel-M4-Reserve-16M-DDR-memory-for-M4-core-use.patch: No such file