Hi,
I am trying to using LTIB for iMX6 Quad SABRE platform.
But currently struck with the error while doing ./ltib
New to the iMX6 environment, can anyone can help.
The error is shown below, Am I missing anything..
Orocessing platform: Host support packages
============================================
using /opt/freescale/ltib/config/platform/host/ltib.preconfig
Processing: fake-provides
===========================
Processing: mkspooflinks
==========================
Processing: distcc
====================
Processing: ccache
====================
Processing: m4
================
Processing: bison
===================
Processing: flex
==================
Processing: texinfo
=====================
Processing: autoconf
======================
Processing: automake
======================
Processing: libtool
=====================
Processing: lkc
=================
Processing: wget
==================
Processing: uclinux-cksum
===========================
Processing: genext2fs
=======================
Processing: genromfs
======================
Processing: gen_init_cpio
===========================
Processing: u-boot-tools
==========================
Processing: mtd-utils
=======================
Build path taken because: no prebuilt rpm,
Testing network connectivity
OK GPP:
Try mtd-utils-1.5.0.tar.gz from the GPP
http://bitshrine.org/gpp/mtd-utils-1.5.0.tar.gz:
12:15:10 ERROR 404: Not Found.
Can't get: mtd-utils-1.5.0.tar.gz at ./ltib line 802.
Died at ./ltib line 1392.
traceback:
main::build_host_rpms:1392
main::host_checks:1447
main:554
Started: Fri Jun 26 12:15:05 2015
Ended: Fri Jun 26 12:15:10 2015
Elapsed: 5 seconds
These packages failed to build:
mtd-utils
Build Failed
Solved! Go to Solution.
Hi Tomas,
Which version BSP are you using? The failed to build mtd-utils it means it can't download the mtd-utils-1.5.0.tar.gz package from GPP.
Here I recommend you refer to Compile L3.0.35_4.1.0 on Ubuntu 14.04 64bit OS document.
If any questions contact me.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Tomas,
Which version BSP are you using? The failed to build mtd-utils it means it can't download the mtd-utils-1.5.0.tar.gz package from GPP.
Here I recommend you refer to Compile L3.0.35_4.1.0 on Ubuntu 14.04 64bit OS document.
If any questions contact me.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Dan,
Thanks for the reply, I proceeding as per the doc specified.
But the command applying patches is giving error.
root@Lijo:/opt/ltib# git apply 0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_14.04_64bit_OS
fatal: can't open patch '0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_14.04_64bit_OS': No such file or directory
root@Lijo:/opt/ltib#
So i get the patch from Compile L3.0.35_4.1.0 on Ubuntu 14.04 64bit OS link Zip file.
But can you mention the procedure to apply the patch manually as the git command didn't work.
Please let me know how to proceed.