i.MX50: Pads for Muxed 16-bit NOR Flash boot mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX50: Pads for Muxed 16-bit NOR Flash boot mode

Jump to solution
1,204 Views
norishinozaki
Contributor V

Hello Champs

I set 00 in BOOT_CFG2[7:6] for muxed 16-bit NOR Flash boot, the data and address pins are connected to the pads in Yellow?

20677_20677.pngpastedImage_0.png

Best regards,

Nori Shinozaki

Labels (1)
0 Kudos
Reply
1 Solution
1,072 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
1,073 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
1,073 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

you are right: EIM_DA[15:0} are used for mode

BOOT_CFG2[7:6]=00  for muxed 16-bit NOR Flash boot

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply